<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>New Products for ADC | Analog Devices</title>
    <link>http://www.analog.com</link>
    <description>New Products for ADC | Analog Devices</description>
    <pubDate>Tue, 23 Apr 2013 16:38:46 GMT</pubDate>
    <dc:date>2013-04-23T16:38:46Z</dc:date>
    <item>
      <title>AD9683, 14位、170 MSPS/250 MSPS、JESD204B模数转换器</title>
      <link>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad9683/products/product.html</link>
      <description>AD9683是一款14位ADC，最高采样速率250 MSPS，旨在为低成本、小尺寸、宽带宽、多功能通信应用提供解决方案。&lt;/p&gt;
&lt;p&gt;这款ADC内核采用多级、差分流水线架构，并集成了输出纠错逻辑。ADC内核具有宽带宽输入，支持用户可选的各种输入范围。集成基准电压源可简化设计。占空比稳定器可用来补偿ADC时钟占空比的波动，使转换器保持出色的性能。JESD204B高速串行接口可降低电路板布线要求，并减少接收器件所需的引脚数量。&lt;/p&gt;
&lt;p&gt;ADC输出数据直接送至JESD204B串行输出通道。这些输出设置为CML电平。数据可以通过通道以最高采样速率250 MSPS发送，得到5 Gbps的通道速率。器件提供同步输入（SYNCINB±和SYSREF±）。&lt;/p&gt;
&lt;p&gt;需要时，灵活的掉电选项可以明显降低功耗。通过专用快速检测引脚支持可编程超量程电平检测。&lt;/p&gt;
&lt;p&gt;设置与控制编程利用三线式S</description>
      <category>ADC</category>
      <category>ADC</category>
      <pubDate>Tue, 23 Apr 2013 16:38:46 GMT</pubDate>
      <guid>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad9683/products/product.html</guid>
      <dc:date>2013-04-23T16:38:46Z</dc:date>
    </item>
    <item>
      <title>AD6677, 80 MH&lt;font style="text-transform: lowercase"&gt;z&lt;/font&gt; Bandwidth, IF Receiver</title>
      <link>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad6677/products/product.html</link>
      <description>AD6677是一款11位、250 MSPS中频(IF)接收机，专门针对要求高动态范围性能、低功耗和小尺寸的电信应用中支持多天线系统而设计。&lt;/p&gt;
&lt;p&gt;该器件包括高性能模数转换器(ADC)和噪声整形再量化器(NSR)数字模块。ADC由多级、差分流水线架构组成，并集成了输出纠错逻辑，每个ADC差分流水线的第一级包含一个宽带宽开关电容采样网络。集成基准电压源可简化设计。占空比稳定器(DCS)补偿ADC时钟占空比的波动，使转换器保持出色的性能。&lt;/p&gt;
&lt;p&gt;ADC的输出内部连接到NSR模块。集成NSR电路能够提高奈奎斯特带宽内较小频段的信噪比(SNR)性能。该器件支持两种不同的输出模式，通过SPI可以选择输出模式。如果使能NSR特性，则在处理ADC的输出时，AD6677可以在有限的部分奈奎斯特带宽内实现更高的SNR性能，同时保持11位输出分辨率。&lt;/p&gt;
&lt;p&gt;可以对NSR模块进行编程，以提</description>
      <category>ADC</category>
      <category>ADC</category>
      <pubDate>Tue, 23 Apr 2013 16:31:55 GMT</pubDate>
      <guid>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad6677/products/product.html</guid>
      <dc:date>2013-04-23T16:31:55Z</dc:date>
    </item>
    <item>
      <title>ADAS3023, 16-Bit 8 Channel Simultaneous Sampling Data Acquisition System</title>
      <link>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/adas3023/products/product.html</link>
      <description>The ADAS3023 is a complete 16-bit successive approximation based analog-to-digital data acquisition system. This device is capable of simultaneously sampling up to 500 kSPS for two channels, 250 kSPS for four channels, 167 kSPS for six channels, and 125 kSPS for eight channels manufactured on the Analog Devices, Inc., proprietary &lt;i&gt;i&lt;/i&gt;CMOS® high voltage industrial process</description>
      <category>ADC</category>
      <category>ADC</category>
      <pubDate>Thu, 28 Mar 2013 09:58:36 GMT</pubDate>
      <guid>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/adas3023/products/product.html</guid>
      <dc:date>2013-03-28T09:58:36Z</dc:date>
    </item>
    <item>
      <title>AD9675, 带JESD204B的八通道超声波AFE</title>
      <link>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad9675/products/product.html</link>
      <description>AD9675支持医疗超声应用，专门针对低成本、低功耗、小尺寸及易用性而设计。它内置8通道的可变增益放大器(VGA)、低噪声前置放大器(LNA)、具有可编程相位旋转功能的CW谐波抑制I/Q解调器、抗混叠滤波器(AAF)、模数转换器(ADC)、数字高通滤波器以及RF2倍射频抽取器。&lt;/p&gt;
&lt;p&gt;每个通道均具有最大52 dB的增益、完全差分信号路径以及有源输入前置放大器终端。通道专门针对高动态范围与低功耗而优化设计，适合要求小尺寸封装的应用。&lt;/p&gt;
&lt;p&gt;LNA具有单端转差分增益，可以通过SPI进行选择。假设噪声带宽(NBW)为15 MHz且LNA增益为21.6 dB，则LNA输入信噪比(SNR)为94 dB。CW多普勒模式下，各LNA输出端驱动一个I/Q解调器。各解调器具有独立可编程的相位旋转和16种相位设置。&lt;/p&gt;
&lt;p&gt;各通道可单独进入省电模式，从而延长便携式应用的电池使用时间。利用</description>
      <category>ADC</category>
      <category>ADC</category>
      <pubDate>Wed, 13 Feb 2013 15:00:55 GMT</pubDate>
      <guid>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad9675/products/product.html</guid>
      <dc:date>2013-02-13T15:00:55Z</dc:date>
    </item>
    <item>
      <title>AD9674, 八通道超声波AFE</title>
      <link>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad9674/products/product.html</link>
      <description>AD9674支持医疗超声应用，专门针对低成本、低功耗、小尺寸及易用性而设计。它内置8通道的可变增益放大器(VGA)、低噪声前置放大器(LNA)、具有可编程相位旋转功能的CW谐波抑制I/Q解调器、抗混叠滤波器(AAF)、模数转换器(ADC)、数字高通滤波器以及2倍射频抽取器。&lt;/p&gt;
&lt;p&gt;每个通道均具有最大52 dB的增益、完全差分信号路径以及有源输入前置放大器终端。通道专门针对高动态范围与低功耗而优化设计，适合要求小尺寸封装的应用。&lt;/p&gt;
&lt;p&gt;LNA具有单端转差分增益，可以通过SPI进行选择。假设噪声带宽(NBW)为15 MHz且LNA增益为21.6 dB，则LNA输入信噪比(SNR)为94 dB。CW多普勒模式下，各LNA输出端驱动一个I/Q解调器。各解调器具有独立可编程的相位旋转和16种相位设置。&lt;/p&gt;
&lt;p&gt;各通道可单独进入省电模式，从而延长便携式应用的电池使用时间。利用待机</description>
      <category>ADC</category>
      <category>ADC</category>
      <pubDate>Fri, 18 Jan 2013 16:52:54 GMT</pubDate>
      <guid>http://www.analog.com/zh/analog-to-digital-converters/ad-converters/ad9674/products/product.html</guid>
      <dc:date>2013-01-18T16:52:54Z</dc:date>
    </item>
  </channel>
</rss>