myAnalog_id
world leader in high performance signal processing
ANALOG
DEVICES
Print     |     Close this window

Network Analyzer

User Interface & Control

  • The Five Motion Senses: Using MEMS Inertial Sensing to Transform Applications (pdf)
  • AN-1057: Using an Accelerometer for Inclination Sensing (pdf)
  • CN0133: Sensing Low-g Acceleration Using the ADXL345 Digital Accelerometer Connected to the ADuC7024 Precision Analog Microcontroller
  • AN-925: Sensors for the AD7147 and AD7148 Captouch® Controllers (pdf)
  • AN-766: Using the Noise Reduction Feature on the AD7877 Touch Screen Controller (pdf)
  • EE-256: Using the ADSP-BF561 Blackfin Processor as a TFT-LDC Controller (pdf)
  • AN-703: Driving High Power LEDs (pdf)
  • AN-738: Using the AD7877 Touch Screen Controller and the Intel PXA250 Processor Under Windows CE.NET (pdf)
  • AN-577: Layout and Grounding Recommendations for Touch Screen Digitizers (pdf)
  • AN-1021: MMSE-Based Multipoint Calibration Algorithm for Touch Screen Applications (pdf)
  • AN-830: Factors Affecting Sensor Response in Captouch® Controllers (pdf)
  • AN-829: Environmental Compensation on the AD7142: The Effects of Temperature and Humidity on Capacitance Sensors (pdf)
  • AN-856: AD7142 Applications Using Sensor Buttons (pdf)
  • AN-645: Interfacing an HD44780 Character LDC to a Microconverter (pdf)
  • AN-908: Interfacing the HD44780-Based Character LCD to an ADUC702X (pdf)
  • AN-601: Minimizing Power Consumption of iMEMS Accelerometers (pdf)
  • AN-1025: Utilization of FIFO Buffer in ADI Digital Accelerometers (pdf)