myAnalog_id
world leader in high performance signal processing
ANALOG
DEVICES
Print
|
Close this window
LCR Meter
User Interface & Control
The Five Motion Senses: Using MEMS Inertial Sensing to Transform Applications
(pdf)
AN-1057:
Using an Accelerometer for Inclination Sensing
(pdf)
CN0133:
Sensing Low-g Acceleration Using the ADXL345 Digital Accelerometer Connected to the ADuC7024 Precision Analog Microcontroller
AN-925:
Sensors for the AD7147 and AD7148 Captouch® Controllers
(pdf)
AN-766:
Using the Noise Reduction Feature on the AD7877 Touch Screen Controller
(pdf)
EE-256:
Using the ADSP-BF561 Blackfin Processor as a TFT-LDC Controller
(pdf)
AN-703:
Driving High Power LEDs
(pdf)
AN-738:
Using the AD7877 Touch Screen Controller and the Intel PXA250 Processor Under Windows CE.NET
(pdf)
AN-577:
Layout and Grounding Recommendations for Touch Screen Digitizers
(pdf)
AN-1021:
MMSE-Based Multipoint Calibration Algorithm for Touch Screen Applications
(pdf)
AN-830:
Factors Affecting Sensor Response in Captouch® Controllers
(pdf)
AN-829:
Environmental Compensation on the AD7142: The Effects of Temperature and Humidity on Capacitance Sensors
(pdf)
AN-856:
AD7142 Applications Using Sensor Buttons
(pdf)
AN-645:
Interfacing an HD44780 Character LDC to a Microconverter
(pdf)
AN-908:
Interfacing the HD44780-Based Character LCD to an ADUC702X
(pdf)
AN-601:
Minimizing Power Consumption of iMEMS Accelerometers
(pdf)
AN-1025:
Utilization of FIFO Buffer in ADI Digital Accelerometers
(pdf)