myAnalog_id
world leader in high performance signal processing
ANALOG
DEVICES
Print     |     Close this window

Healthcare - MRI

Circuits From the Lab

  • Using the AD8352 as an Ultralow Distortion Differential RF/IF Front End for High Speed ADCs (CN0046)
  • Interfacing the ADL5382 Quadrature I/Q Demodulator to the AD9262 16-Bit Continuous Time Sigma-Delta ADC as an RF-to-Bits Solution (CN0062)
  • Using the AD8376 VGA to Drive Wide Bandwidth ADCs for High IF AC-Coupled Applications (CN0002)
  • Very Low Jitter Encode (Sampling) Clocks for High Speed Analog-to-Digital Converters Using the ADF4002 PLL (CN0003)