MATLAB Compiler

1. Prerequisites for Deployment 

. Verify the MATLAB Compiler Runtime (MCR) is installed and ensure you    
  have installed version 7.17 (R2012a).   

. If the MCR is not installed, do following:
  (1) enter
  
      >>mcrinstaller
      
      at MATLAB prompt. This MCR Installer command displays the 
      location of the MCR Installer.

  (2) run the MCR Installer.

Or download Windows 64bit version of MCR from the MathWorks website:

   http://www.mathworks.com/products/compiler/
   
   
For more information about the MCR and the MCR Installer, see 
Working With the MCR in the MATLAB Compiler Users Guide.    


NOTE: You will need administrator rights to run MCRInstaller. 


2. Files to Deploy and Package

Files to package for Standalone 
================================
-beamforming64.exe
-MCRInstaller.exe 
   -include when building component by clicking "Add MCR" link 
    in deploytool
-This readme file 

3. Definitions

For information on deployment terminology, go to 
http://www.mathworks.com/help. Select your product and see 
the Glossary in the Users Guide.