*****************************************************************************************


This ZIP File is associated with Rev 1 of the Application Note


    Static Voltage Scaling for ADSP-2148x SHARC Processors  (EE-357)  


that can be found at http://www.analog.com/ee-notes


Date Created:	Mar 22nd, 2013


*****************************************************************************************


This package includes the following files:

1. The example 2148x_SVS_example_code.c and associated project file

2. The schematics and board design database for the ADSP-2148x SVS EZ-BuB

3. The Bill-of-materials (BOM) for the ADSP-2148x SVS EZ-BUB

4. The Excel spreadsheet for AD5258 digipot step calculation for VDD_INT


*****************************************************************************************

Please note that in the associated files, the acronyms "SVS (static voltage scaling)" 
and "AVP (automatic voltage positioning)" are sometimes used interchangably and are 
meant to represent the same concept.

All code examples have been written and tested with

	VisualDSP++ 5.0 Update 10

	ADSP-21489 revision 0.0

	EZ-BUB revision 0.1


*****************************************************************************************