******************************************************************************

This ZIP File is associated with Rev 2 of the Application Note

        Using the ADSP-BF592 Blackfin Processor Tools Utility ROM (EE-351)

that can be found at http://www.analog.com/ee-notes

Date Created:   March 16, 2011


******************************************************************************


This EE-Note describes the Tools Utility ROM and explains how it could
be used to reduce the amount of L1 instruction SRAM that an application
uses. It also discusses the implications of using the ROM.

The accompanying spreadsheet identifies the C and DSP run-time library
functions that are installed in Tools Utility ROM for silicon revision 0.1
and 0.2 of the ADSP-BF592 Blackfin Processor; however the spreadsheet does
not include the compiler support routines or TMK (the core of VDK - the
VisualDSP++ RTOS) that are also part of the ROM.


******************************************************************************


All code examples have been written and tested with

	VisualDSP++ 5.0 Update 9

	ADSP-BF592 revision 0.2

	EZ-KIT Lite revision 0.1


*****************************************************************************************