/*************************************************************************************************************************************************/

This code configures the primary SPI of the ADSP-21369 SHARC processor in slave mode. The SPI is configured as transmitter or receiver based on the
macro settings in SPI.h file. When configured as receiver after the DMA is completed the data received is compared with the known data.
In case of failure only one LED is toggled and for the passing case 3 LEDs on the ADSP-21369 EZ-KIT Lite board are toggled. 

The following are the files available in the project:

1. SPI.h file which has the macros for configuring the system and SPI.  
	a. The SET_CPHASE, SET_CLKPL and SET_CPHASE_CLKPL macros are used for selecting Clock Phase and Polarity for the SPI transfers. 
	b. Using the SL_TRANSMITTER macro the SPI can be configured as transmitter in DMA mode otherwise the SPI is used as receiver in DMA mode. 
	c.The core clock for the ADSP-21369 processor also can be defined using the PLL_XXX_MHZ macros. These macros allow the processor to run in the 
	configured core clock. The PMCTL register is configured as per the macro value selected.
	
2. Configdai.asm which has the SRU routings for the SPI. The SPI signals are routed as follows:
	a. DPI 6 - SPI_CLK
	b. DPI 7 - SPI_MOSI		
	c. DPI 14 - SPI_DS
	d. DPI 13 - SPI_MISO
	
3. InitPLL.asm - Configures the PLL as per the Core clock frequency selected.

4. SPI_Slave_DMA.asm - Configures the SPI control registers for slave mode DMA operation. 
						  
/*************************************************************************************************************************************************/