*****************************************************************************************


This ZIP File is associated with Rev 1 of the Application Note


    Using Blackfin Processor Hibernate State for Low Standby Power (EE-334)  


that can be found at http://www.analog.com/ee-notes.


Date Created:	April 30th, 2008


*****************************************************************************************


The archive provides 2 code examples:

BF533_EZKIT_Hibernation_Example.dpj in directory /BF533_EZKIT_Hibernation_Example
illustrates use of the ADSP-BF533 EZ-KIT Lite evaluation system to place the processor
into the hibernate state and wake up due to a Real-Time Clock interrupt.

PMP_Hibernation_Example.dpj in directory /PMP_Hibernation_Example is the same project
used for a customized PMP board that employs the additional hardware and GPIO control
described in EE-334.


*****************************************************************************************


All code examples have been written and tested with

	VisualDSP++ 4.5 Update 6

	ADSP-BF533 revision 0.5

The BF533_EZKIT_Hibernation_Example.dpj project was tested with

	ADSP-BF533 EZ-KIT Lite revision 2.1


*****************************************************************************************