****************************************************************************************************
ADSP-BF561 Video templates

EE-xxx - "Video Templates for Developing Multimedia Applications on Blackfin"

Analog Devices, Inc.
DSP Division
Three Technology Way
Norwood, MA 02062

Date Created:	08/08/2006

Check for latest updates of the software on the following page: 

"http://www.analog.com/processors/blackfin/technicalLibrary/applicationNotes/index.html"


Version Info: 
ADSP-BF561 EZ-KIT Lite 1.4
Silicon Rev. 0.5
VisualDSP++ 5.0
****************************************************************************************************

The folder contains the sources for three templates  dicussed in the EE- note and 
a utilities folder.

The sources for the templates are located in <template name>/BF561/template
for example in case of line_proessing is in  <Line_processing>/BF561/template

The example projects are also organized in a similar way. The sources for the
example projects are located in <template name>/BF561/example.

Please note that the examples are only provided to demonstrate the use of templates.
They are not for complete demonstration purposes.

The ./utilities folder contains the following files:
"./ezkitutilities.c",
"./ezkitutilities.h",
"./video.c",
"./video.h"

A readme file is available for each of the projects to discuss specifics of the projects.

For detailed description of the templates please refer to the accompanying EE- note.