File Name: SPI_Slave.ldr
_____________________________________________________________________________________

Hardware settings:
BMODE[1:0] = 10
_____________________________________________________________________________________

This loader file shoud be sent by an SPI Master device to the ADSP-BF561 processor. It 
would demonstrate the SPI Slave boot mode of the ADSP-BF561 processor.
_____________________________________________________________________________________
	
Functional Overview:
This project blinks both rows of LEDs on the EZ-KIT Lite board when the RESET signal
is de-asserted (Reset button on the EZ-KIT Lite board released). CoreA blinks one row
while coreB blinks the other.
_____________________________________________________________________________________	

Note: You could use the ADSP-BF533 processor as the host device to test this mode. The 
code for the same is available in the accompanying software code of the Application
Note, EE-240