Project Name: No_boot_mode
_____________________________________________________________________________________

Hardware settings:
BMODE[1:0] = 00
_____________________________________________________________________________________

This project demonstrates the No-boot mode of the ADSP-BF561 processor.
_____________________________________________________________________________________
	
Functional Overview:
This project blinks LEDs on the EZ-KIT Lite board when the RESET signal
is de-asserted (Reset button on the EZ-KIT Lite board released).
_____________________________________________________________________________________	

Operation description:


- Open the project "No_boot_mode.dpj" in the VisualDSP Integrated Development 
  Environment (IDDE).
- Build the project. A loader file, N0_boot_mode.ldr is generated.
- Use the Flash Programmer utility to burn the Loader file into Flash.
- Disconnect the target in the VDSP++ session.
- Check BMODE pins are set to 00. On the EZ-KIT Lite board, verify that SW3 position1,
  position 2 are ON.
- Press reset and release.

Both rows of LEDs on the board will toggle. The settings in the project options to be 
used are shown in the folder ./Screen-shots
_____________________________________________________________________________________