****************************************************************************

This Source Example is associated with Rev 1 of the Application Note


    Interfacing NAND Flash Memory with ADSP-2126x SHARC Processors (EE-279)  


that can be found at http://www.analog.com/ee-notes.




Analog Devices, Inc.
DSP Division
Three Technology Way
P.O. Box 9106
Norwood, MA 02062

Date Created:	11/17/2005
----------------------------------------------------------------------------

Description of the EE-Note:

The objective of NAND Flash is to provide an alternative to the hard disks especially in 
the case of portable and handheld systems. Cellular phones, personal digital assistants 
(PDA), digital cameras, MP3 players and other mobile computing, communications, and 
consumer products use FLASH memory as the primary storage media. Applications use NAND 
Flash memory to store information such as images, data, and music therefore requiring 
much higher density. This application note provides details on how to interface NAND Flash 
memory to the ADSP-2126x SHARC DSP Processors especially considering the fact that the 
ADSP-2126x does not have a NAND flash controller on-chip and also that its parallel port 
has multiplexed address and data signals. This interface is demonstrated by code examples 
which are validated on EZ-KIT Lite platform. The memory device part number used to 
demonstrate this interface is K9F1208U0B, manufactured by Samsung Electronics. 
-----------------------------------------------------------------------------
Zip file contents are:

1. NAND With ADSP-21262 :: This contains the example code and screenshots of VDSP



-----------------------------------------------------------------------------

VisualDSP++ version : VisualDSP++ 4.0


-----------------------------------------------------------------------------