********************************************************************************************

This code example accompanies application note

  Programming Asynchronous Sample Rate Converters on ADSP-2136x SHARC Processors (EE-268) 

that can be found on http://www.analog.com/ee-notes.


Analog Devices, Inc.
DSP Division
Three Technology Way
P.O. Box 9106
Norwood, MA 02062

Date Created:	Apr 15, 2005

-------------------------------------------------------------------------------------

Description of the EE-Note:

This application note explains the fundamentals of sample rate conversion and demonstrates
with examples how to program the sample rate converters of ADSP-2136x SHARC DSP processors.
The code examples provided with this application note also demonstrate the Signal Routing 
Unit (SRU) programming required to interface the sample rate converter (SRC) with the 
serial ports (SPORTs) of ADSP-21364. A real time code example supplied with this 
application note demonstrates a simple talk-through code with various sample rate ratios.

 
-------------------------------------------------------------------------------------

1. Example set-up I - This folder has code for SRC example set-up I explained in the EE note.
2. Example set-up II - This folder has code for SRC example set-up II explained in the EE note.
		       This is a real time code with data in/out from / to codec on the EZ-KIT Lite.


-------------------------------------------------------------------------------------

Software written for VisualDSP++ 3.5 (November update)