*****************************************************************************************

Interfacing AD7865 Parallel ADCs to ADSP-2136x SHARC Processors (EE-260)

Analog Devices, Inc.
DSP Division
Three Technology Way
P.O. Box 9106
Norwood, MA 02062

Date Created:	27/11/2004
----------------------------------------------------------------------------
Description of the EE-Note:

This Application note  explains how to interface parallel ADCs to ADSP-21365 SHARC processors.
The parallel ADC considered in this application note is AD7865. This application note also 
provides example code to demonstrate how the SHARC processors parallel port can be programmed 
to receive data from AD7865 in parallel port DMA mode.


----------------------------------------------------------------------------
There are two sub folders :
1. ADSP-21365_with_AD7865_DMA : this contains code for the DMA interface on
DSPs's parallel port.
2. ADSP-21365_with_AD7865_PDAP : this contains code for the interface on DSP's Parallel 
Aquisition Port -  PDAP.

-----------------------------------------------------------------------------
Software written for VisualDSP++ 3.5