*****************************************************************************************

Interfacing AD7865 Parallel ADCs to ADSP-21161 SHARC Processors (EE-259)  

Analog Devices, Inc.
DSP Division
Three Technology Way
P.O. Box 9106
Norwood, MA 02062

Date Created:	27/11/2004
----------------------------------------------------------------------------

Description of the EE-Note:
This Application note  explains how to interface parallel ADCs to ADSP-21161 SHARC processors. 
The parallel ADC considered in this application note is AD7865. This application note also 
provides example code to demonstrate how the SHARC processors external port can be programmed 
to receive data from AD7865 in core and DMA modes.


----------------------------------------------------------------------------

This zip file contains the following two folders:

1. ADSP-21161_with_AD7865_Core
	: This folder contains example code in core mode.
2. ADSP-21161_with_AD7865_DMA
	: This folder contains example code in DMA mode.

-----------------------------------------------------------------------------

Software written for VisualDSP++ 3.5