These are the files that are associated with the application note

	A Boot Compression/Decompression Algorithm for Blackfin Processors (EE-257)

that can be found at http://www.analog.com/ee-notes


"Compression Program BF533" folder: Algorithm for use with ADSP-BF533 single-core processors
"Compression Program BF561" folder: Algorithm for use with ADSP-BF561 dual-core processors
"Utilities" folder: program and script to convert ASCII files into Intel Hex format

The code included with this note was verified using VisualDSP++ 3.5 (September update) for Blackfin 
and the project was run on the EZ-KIT Lite evaluation systems for both the ADSP-BF533 (Si. Rev. 0.2) 
and the ADSP-BF561 (Si. Rev. 0.2) Blackfin Processors (ADDS-BF533-EZLITE, board Rev 1.2 and 
ADDS-BF561-EZLITE, board Rev 1.1).

(c) 2004 Analog Devices Inc. All rights reserved.