This folder contains the software code for the application note 

	Interfacing ADSP-21365 SHARC PDAP to ADSP-BF533 Blackfin EBIU (EE-254)

The software implements the data transfer protocol between the ADSP-21365 and ADSP-BF532 as mentioned 
in the application note. The ADSP-21365 and ADSP-BF532 should have hardware connections as depicted 
in the figure.2 of the application note. The folder contains two subfolders:--

	(a) "EBIU driver code" containing the driver software for the ADSP-BF532.
	(b) "PDAP driver code" containing the driver software for the ADSP-21365.

All software was tested with VisualDSP++ 3.5.


(c) Analog Devices Inc. 2004