****************************************************************************
Interfacing AD7676 ADCs to ADSP-21365 SHARC Processors (EE-248)   

Analog Devices, Inc.
DSP Division
Three Technology Way
P.O. Box 9106
Norwood, MA 02062

Date Created:	27/9/2004
----------------------------------------------------------------------------

Description of the EE-Note:

This application note explains in detail a scheme to interface AD7676 ADC in 
Master Serial Mode (Internal discontinuous clock) with SHARC ADSP-21365 DSP. 
This application note also provides example code to demonstrate how ADSP-21365 
Serial Port can be programmed in order to receive data from AD7676 while AD7676 
converter is configured in master serial mode supplying discontinuous serial 
data clock to the DSP serial port. 
-----------------------------------------------------------------------------

The current directory contains folder "Interfacing ADSP-21365 with AD7676" which 
contains the code.



-----------------------------------------------------------------------------

Visual DSP version : VisualDSP++3.5 (July update)

ADSP-21365 Evaluation board.


-----------------------------------------------------------------------------