*****************************************************************************************


This ZIP File is associated with Rev 2 of the Application Note


    In-Circuit Programming of an SPI Flash with SHARC Processors (EE-231)  


that can be found at http://www.analog.com/ee-notes.


Date Created:	Aug 22th, 2007


*****************************************************************************************


The archive provides two code examples:

Example 1 in directory ADSP-21262 illustrates programming the SPI Flash M25P20 using the
ADSP-21262 SHARC processor

Example 2 in directory ADSP-21364 illustrates programming the SPI Flash M25P20 using the 
ADSP-21364 SHARC processor

*****************************************************************************************


All code examples have been written and tested with

	VisualDSP++ 4.5 June 2007 update

	ADSP-21262 EZ-KIT Lite revision 2.0

        ADSP-21364 EZ-KIT Lite revision 2.0


*****************************************************************************************