___________________________________________________________________________
README      EE-230

Analog Devices, Inc.
DSP Division
P.O. Box 9106
Norwood, MA 02062

11-APR-2005

This directory contains a collection of simple blink program to demonstrate the use of code
overlays on the Third Generation SHARC families using VisualDSP++(R).

The code examples included in the subdirectories were generated using VisualDSP++ version 3.5
and are forward compatible with VisualDSP++ version 4.0. The code can be executed as is on any
ADSP-21262 EZkit Lite or ADSP-21364 EZKit Lite. Please make sure that the LED_CS_SW switch
is set to its OFF position before running the code (see the EZKit schematic included with the
EZKit user's manual).

In general, these examples apply to any revision of any of the following processors...

ADSP-21261
ADSP-21262
ADSP-21266
ADSP-21363
ADSP-21364
ADSP-21365
ADSP-21366

In addition, the basic concepts will apply to the ADSP-21367/8/9 with minor changes being
necessary in the overlay manager to access the peripherals being used.