*****************************************************************************************


This ZIP File is associated with Rev 2 of the Application Note


    In-Circuit Flash Programming on SHARC Processors (EE-223)  


that can be found at http://www.analog.com/ee-notes.


Date Created:	Feb 19th, 2007

*****************************************************************************************

The archive provides the following code examples:

1. 21161 - The following projects in this folder illustrate Flash programmer for the 
ADSP-21161 processor:
        1. Blink - Example LED blink code.
        2. Flash programmer - Flash programmer project for ADSP-21161

2. 21262 - The following projects in this folder illustrate Flash programmer for the
ADSP-21262 processor:
	1. Blink - Example LED blink code.
        2. Flash programmer - Flash programmer project for ADSP-21262
	  
*****************************************************************************************

The ADSP-21161 code examples have been written and tested with

	VisualDSP++ 4.5 Novemember 2006 Update

	ADSP-21161 revision 1.2 EZ-KIT Lite revision 2.3

The ADSP-21262 code examples have been written and tested with

	VisualDSP++ 4.0 December 2005 Update

	ADSP-21262 revision 0.1 EZ-KIT Lite revision 1.2
	
	Note that the Visual DSP++ 4.0 supports initializing the external variables on the 
	parallelport external SRAM. But in VDSP 4.5 the external memory access for the 2126x
	and 21362/3/4/5/6 processors are changed. The linker can not directly initialize the
	data to the external memory.This example code can not be tested as it is on the 
	Visual DSP++ 4.5 version.
	

*****************************************************************************************