*****************************************************************************************


This ZIP File is associated with Rev 3 of the Application Note


    SHARC SPI Slave Booting (EE-177)  


that can be found at http://www.analog.com/ee-notes.


Date Created:	Jan 19th, 2007


*****************************************************************************************


The archive provides the following code examples:

The Boot_kernel directory contains the modified boot kernel projects for all processors:

      a. 161_spi - This folder has the modified SPI boot kernel for the ADSP-21161 processor.
      b. 26x_spi - This folder has the modified SPI boot kernel for the ADSP-2126x processors.
      c. 36x_spi - This folder has the modified SPI boot kernel for the ADSP-21362/3/4/5/6
      	 processors.
      d. 369_spi - This folder has the modified SPI boot kernel for the ADSP-21367/8/9
      	 processors.

The SPI Host directory contains the SPI Host example code for the ADSP-21161 processor.


*****************************************************************************************


All code examples have been written and tested with

	VisualDSP++ 4.5 November Update

	ADSP-21161 revision 1.2

	EZ-KIT Lite revision 2.3
	
	ADSP-21262 revision 0.1
		
	EZ-KIT Lite revision 1.5
		
	ADSP-21364 revision 0.5
	
	EZ-KIT Lite revision 1.1
		
	ADSP-21369 revision 0.1
		
	EZ-KIT Lite revision 1.2


*****************************************************************************************