*****************************************************************************************


This ZIP File is associated with Rev 2 of the Application Note


     Understanding and Using Linker Description Files on SHARC processors (EE-069)    


that can be found at http://www.analog.com/ee-notes.


Date Created:	Jan 17th, 2007


*****************************************************************************************

Example 1 in directory 21065L_LDF_Example contains an ADSP-21065L project file which
explains how to place various functions into different memory locations using LDF commands.

Example 2 in directory 21375_LDF_Example contains an ADSP-21375 project file which
explains how to place various functions into different memory locations using LDF commands.

*****************************************************************************************

All code examples have been written and tested with

	VisualDSP++ 4.5 November Update

	ADSP-21065L revision 0.3

	EZ-KIT Lite revision 2.03
	
	ADSP-21375 revision 0.0
	
	EZ-KIT Lite revision 1.0


*****************************************************************************************