![]() |
|
| Home Analog Devices Feedback Subscribe Archives 简体中文 日本語 | |
|
|
|
|
ADIsimPower Provides Robust, Customizable DC-to-DC Converter Designs Introduction While most dc-to-dc selection guides simply direct users to switching regulators, switching controllers, and linear regulators that will work with a given set of inputs—without providing the means to quantify the trade-offs made in selecting one part over another—ADIsimPower allows designers to investigate power-conversion trade-offs and navigate design complexities. An intelligent selection guide combined with a comprehensive design assistant, this new tool provides robust designs that are optimized to the user's exact inputs for size, efficiency, cost, parts count, or some combination thereof. The ADIsimPower selection and design process comprises four steps: 1. Enter Your Design Criteria, 2. View All Design Solutions, 3. View Solution Details, and 4. Build Your Design. At the end of the experience, the goal is for ADIsimPower to provide a customized schematic, bill of materials (BOM) with vendor part numbers and prices, efficiency plots, performance specifications, closed-loop transfer function, and the means to rapidly build the design.
Enter Your Design
Criteria Or, users who know which Analog Devices power management part they would like to use can select choose the IC. This will activate a pull-down menu that displays a list of currently supported power management ICs. After selecting one of these parts, the user will be taken directly to View Solution Details.
View All Design
Solutions Below the Recommended Solutions, a table quantifies to the first order the solution cost, size, efficiency, and component count for every IC that works, allowing users to see the design trade-offs without having to do individual designs with each part. Each column can be sorted to highlight the most important trade-offs. A feature list can be found at the right of the table. To expand or collapse this list, click on Show all features or Show default features. Clicking on the associated check box selects or deselects a feature. Select all the features that are required for the application. ICs that do not include the selected features will be removed from the table and from the recommended solutions.
After selecting the IC that best balances features, performance, integration level, and cost, click on the corresponding View Solution button. If this button is not active, comprehensive design support is not yet available on ADIsimPower. Click on the IC name to see the data sheet and other information. Click Download Design Tool to get an Excel-based design tool that can be run locally. View Solution
Details At the top of the page, the original inputs are repeated for clarity; they can be updated if the design parameters have changed. Click on Modify Advanced Settings, which will open up a window allowing the user to modify many settings, including, but not limited to, accuracy, maximum component height, peak-to-peak output voltage ripple, input filter requirements, load transient response, inductor ripple current, and MOSFET vendor preference (a subset of these features may be shown depending upon the part selection). The ability to modify these settings is one way in which ADIsimPower differentiates itself from other dc-to-dc converter design tools. Though understandable enough to make novice power supply designers feel comfortable, the advanced settings are exactly the kind of parameters expert power supply designers expect to control in their designs. The next section on the page has several tabs that specify various important design parameters. Once again, the information in these tabs will vary depending upon the chosen IC, but common tabs include Operational Estimates, Dissipation Estimates, and Temperature Estimates. All parameters are shown at both minimum and maximum input voltage. The Operational Estimates tab includes parameters such as PWM duty cycle, peak-to-peak output voltage ripple, and peak inductor current. The Dissipation Estimates tab shows the power dissipated in each high loss component. The Temperature Estimates tab shows the temperatures of each of the components associated with loss in the Dissipation Estimates tab. Power dissipation and temperature calculations assume worst-case values for many of the parameters that dictate power loss to ensure a robust design. The following section shows the complete customized schematic, including reference designations and pin numbers.
Next on the page is the Bill of Materials. This may have several components that can be edited, as indicated by an orange item number. Click on the item number to see a list of other components that are prequalified to work in the design. The column headings will vary depending upon the type of component. Typical headings include Manufacturer, Part Number, Loss (W), Area (mm2), Hgt (mm), Cost ($), and other specifications that characterize the part and how it will work in the circuit. These allow the user to continue to make performance-vs.-size-vs.-cost trade-offs to fully customize the design. Each of these columns can be sorted, which makes quantifying gains and losses associated with changing parts easier. If a new part is selected, ADIsimPower will redesign with the selected component, ensuring that all specifications are still met.
Below the Bill of Materials is the Graphs section, which may include plots of efficiency, loss, and the closed-loop transfer function (Bode plot)—all at both minimum and maximum input voltages. The efficiency and loss curves correspond to losses associated with worst-case values for many high loss parameters. This worst-case analysis is common throughout the ADIsimPower design process. The goal is to give the user confidence that the designs provided by the tool are robust across component tolerances, ambient temperature range, and other circuit variances. This tool provides far more than a basic solution. At the top of each section in the View Solution Details stage are radial buttons for each design criterion (Lowest cost, Part count, Efficiency, and Size). Selecting a new radial button will completely redesign the circuit according to the new design criteria, nullifying all BOM changes previously made. When the final design has been determined, click on Build This Solution!
Build Your Design Links allow the user to download or email all information found in the Build Your Design and View Solution Details sections in a format similar to that seen while interacting with the tool on the Web. Parts Database
Conclusion
|
||||||