![]() |
|||
![]() |
![]() |
![]() |
![]() |
|
Volume 34, Number 05, August-September, 2000
VDSL Technology IssuesAn Overview
Abstract
1. Introduction
2. VDSL deployment configurations
Figure 1a. FTTEx configureation
The present spectrum allocation proposals use the ADSL downstream frequency band for VDSL downstream as well. From the point of view of the crosstalk between ADSL and VDSL, there is a subtle difference between the two configurations of Figure 1. In the FTTEx case the presence of the VDSL does not affect ADSL performance, because VDSL power spectral density (PSD) is less than ADSL PSD. Conversely, the presence of ADSL in the same binder may have a serious impact on VDSL performance. In FTTCab configuration the situation is reversed. VDSL signals from the ONU may generate unacceptable noise levels for the ADSL downstream signal, as it becomes heavily attenuated along the path from CO to ONU [1].
3. Data rates and spectrum allocation
The asymmetrical services expected to dominate in the US market include video distribution-including HDTV-and Internet applications. In Europe there is more interest in the symmetrical services, which are directed towards business applications. Within each category of services, the data rate depends on the distance from the customer premises to the ONU (CO). Frequency-division multiplexing (FDM) was chosen as the multiplexing method for separating the upstream and downstream data transmission. For asymmetrical services the ratio between the downstream and upstream data rate is close to 10:1, thus most of the bandwidth should be allocated for downstream. For symmetrical services the bandwidth should be allocated equally to the two directions. A requirement of the standards is that both types of services should coexist on the same cable. Under these conditions, no spectral allocation method can simultaneously optimize both the asymmetrical and symmetrical services data rates. One solution is to define two spectrum allocations: One is optimized toward the asymmetrical services, while accommodating certain symmetrical data rates as a secondary goal; the other is geared more towards symmetrical services. Also, because the short loop profile requires considerable bandwidth, it was recognized that it will be difficult to accommodate them in the same binder with the rest of the services. This is why the standardization effort is presently focused on medium loop profiles; this spectral allocation is also suitable for the long loop case. An agreement in principle was reached within ITU for a spectrum allocation which contains 4 bands (two downstream and two upstream) in the 138-kHz-to-12-MHz frequency range. An example of such a spectrum allocation for North America [2] is shown in Figure 2. The reach is 2500 ft for 22/3 Mb/s asymmetrical services and 1700 ft for 13/13 Mb/s symmetrical services. For lower data rates on longer loops the first upstream/downstream bands can be used. Future allocation of the spectrum above 12 MHz will allow the transmission of higher data rates on short loops.
Figure 2. VDSL frequency plan for North America
4. Bridged taps
Figure 3. Magnitude response of a bridged-tap loop.
5. Crosstalk noise sources
Figure 4. Twisted-pair crosstalk noise sources.
The far-end crosstalk (FEXT) noise is generated between signals travelling in the same direction in a cable. FEXT is the dominant crosstalk noise source in VDSL. Its power spectral density: depends on the frequency, f, the length of the cable segment, L, that the two signals run in parallel, and the channel transfer function Hch(f). Because the channel transfer function is an exponential function of L, the power spectral density of the FEXT noise is small for large values of L and is relatively high for low L. In the upstream direction (Figure 4), transmitter Tx4US is much closer to ONU than Tx2US and Tx3US. Tx4US will inject a relatively high level of FEXT noise in pairs2 and 3. The upstream signals from these pairs are heavily attenuated at the point where the FEXT noise is injected. The result is that in the upstream direction the FEXT noise from sources close to the ONU (CO) will degrade significantly the SNR of the sources far away from ONU, collocated in the same binder. The solution consists in reducing the transmit power, depending on the distance from the transmitter location to the ONU(CO). This problem does not exist in the downstream direction (all the transmitters are located at ONU/CO).
6. RF interference
Three proposals for the line-code were submitted to the standards organizations:
QAM and DMT modulation are compared below in the light of VDSL's specific problems. In most of the cases the reader will be able to extrapolate the results for FMT. The DMT signal has a gaussian amplitude distribution. A peak-to-average ratio (PAR) of 15 dB is necessary to reduce the clipping to an acceptable level. Accommodating such high signal peaks requires an extended range for the transmitter buffer and increases the power consumption in the analog front end. Some of the single-carrier modulation's advantage is lost, because the line signal is the sum of two QAM channels (see Figure 2). Two QAM transmitters/receivers are necessary in each direction for single-carrier modulation; the DMT requires frame synchronization and supervision; and timing recovery is more difficult. As a result the complexity is about the same for the two methods. The data rate losses due to cyclic prefix/suffix (DMT modulation) and guard bands (QAM) are similar. RF egress. In order to reduce the transmit PSD to -80 dBm/Hz for each of the radio amateur bands falling within the transmit band, notch filters are necessary for single modulation systems. These filters make the equalization more difficult. In DMT systems, the bins falling within amateur radio bands are not used. As a general observation, DMT modulation's greater flexibility in controlling PSD across the VDSL spectrum may translate into a higher performance. VDSL allows the transmission of high data rates, up to 52 Mb/s, using the existing twisted-pair wires. An agreement was reached in the standards organizations on using frequency division multiplexing with four frequency bands (two for upstream and two for downstream) in the138-kHz-to-12-MHz frequency range. The details of the spectrum allocation are yet to be firmed up. The FEXT noise is the major crosstalk impairment. It requires power-back off in the upstream direction. Short bridged taps can significantly alter the ratio between the upstream and downstream data rate, this is the reason they are not specified in the ETSI standard; however they are still part of the US standard. Finally, T1E1 and ETSI agreed to include all three line codes in the present standards. In the long term the standards may evolve to the line code most capable of facing the difficult technical problems posed by VDSL.
|
|||||||||||||||||||||||||||||||