|
1.5-W Loudspeaker Amplifier Delivers Sound Performanceby Troy Murphy The SSM2211 speaker amplifier, from the Analog Devices audio amplifier group, is an operational power amplifier designed to deliver up to 1.5 W of power into a 4-
At maximum output power, the total harmonic distortion (THD) is only 0.1%, a significant improvement over IC speaker amplifiers currently on the market. Design objectives There are two major challenges in designing a power amplifier to be housed in a small-outline (SOIC) package. One is to deliver the maximum power efficiently from a single supply voltage. The other is to dissipate the heat the device generates at high output power levels without excessive temperature rise. To drive a load connected from the single-ended output of an amplifier to ground, the maximum sine-wave power available is simply VP2/(2R), where VP is the peak voltage. In the ideal case (rail-to-rail), VP would be half the supply voltage, and max output would be Vs2/(8R). With the amplifier biased halfway in a single-supply application, a capacitor must be used to couple a speaker to a single-ended output to block direct current from the speaker. Because the typical resistance of a speaker can be 8 By connecting a speaker across both outputs in a pushpull, or bridge-tied load (BTL) configuration, the need for a coupling capacitor is eliminated, because both output terminals are biased to the same dc voltage. The BTL configuration also doubles the voltage swing across the output. Because the output power is proportional to the square of the voltage, this allows four times as much power to be delivered to the speaker, a loudness increase of 12 dB. In addition, efficiency can be greater. The maximum power dissipation of the SSM2211 is a function of the supply voltage and the resistance of the speaker it is driving. It can be found by the formula:
where VDD is the supply voltage and RL is the speaker resistance. With a +5-V supply and an 8-ohm speaker, the maximum power dissipation of the device is 633 mW. This can result in a significant heat increase in a standard SO-8 package. To improve the heat dissipation from the package, the SSM2211 uses a modified package for lowered thermal resistance. This proprietary package, developed by Analog Devices, uses an internal modification called a Thermal Coastline® to improve the thermal resistance in a SOIC package by more than 30%.
For standard SOIC package, typical junction-to-ambient-termperature thermal resistance (thetaJA) is 158 °C/W. In a Thermal Coastline SOIC package, thetaJA is 98°C/W. Thus, a die in a Thermal Coastline package will not get as hot as a die in a standard package with the same power dissipation. As a result of this packaging, SSM2211 can deliver 1 W into an 8- Analog Devices Termal Coastline technology is not limited to small outline packages; it can be applied to practically any package type. Besides high-power audio, these new thermally efficent packages have useful applications in power management and temperature sensing devices. You can expect to see more small packages of this sort with greater power output on increasing numbers of new products from Analog Devices. |
|||||||||