Ask The Applications Engineer -12
GROUNDING (AGAIN)
by Walt Kester
Q. Ive read your data sheets and application notes and also attended your seminars, but Im still confused about how to deal with analog (AGND) and digital (DGND) ground pins on an ADC. Your data sheets usually say to tie the analog and digital grounds together at the device, but I dont want the ADC to become my systems star ground point. What do I do?
A. First of all, dont feel bad that you are confused about what to do with your analog and digital grounds. So are lots of folks! Much of the confusion comes from the labeling of the ADC ground pins in the first place. The pin names, AGND and DGND, refer to whats going on inside the component itself and do not necessarily imply what you should do with them externally. Let me explain.
Inside an IC that has both analog and digital circuits, such as an ADC, the grounds are usually kept separate to avoid coupling digital signals into the analog circuits. The diagram shows a simple model of an ADC. There is really nothing the IC designer can do about the wirebond inductance and resistance associated with connecting the pads on the chip to the package pins. The rapidly changing digital currents produce a voltage at point B which will inevitably couple into point A of the analog circuits through the stray capacitance. Its the IC designers job to make the chip work in spite of this. However, you can see that in order to prevent further coupling, the AGND and DGND pins should be joined together externally to the same low impedance ground plane with minimum lead lengths. Any extra external impedance in the DGND connection will cause more digital noise to be developed at point B; it will, in turn, couple more digital noise into the analog circuit through the stray capacitance. Though an extremely simple model, this serves to illustrate the point.

Q. O.K., youve told me to join the AGND and DGND pins of the IC together to the same ground plane-but I am maintaining separate analog and digital ground planes in my system. I want them tied together only at one point: the common point where the power supply returns are all joined together and connected to chassis ground. Now what do I do?
A. If you have only one data converter in your system, you could actually do what the data sheet says and tie your analog and digital ground systems together at the converter. Your system star ground point is now at the data converter. But this may be extremely undesirable, unless you initially planned your system with this thought in mind. If you have several data converters located on different PCBs, the concept breaks down, because the analog and digital ground systems are joined at each converter on a number of PCBs. This is a perfect invitation for ground loops!
Q. I think Ive figured it out! If I must join the AGND and DGND pins together at the device, and I want to maintain separate system analog and digital grounds, I tie both AGND and DGND to either the analog ground plane or the digital ground plane on the PCB, but not both. Right? Now, which one should it be, since the ADC is both an analog and a digital device?
A. Correct! Now, if you connect the AGND and DGND pins both to the digital ground plane, your analog input signal is going to have digital noise summed with it, because it is probably single-ended and referenced to the analog ground plane.
Q. So the right answer is to connect both AGND and DGND pins to the analog ground plane? But doesnt this inject digital noise on my nice quiet analog ground plane? And isnt the noise margin of the output logic degraded because it now referenced to the analog ground plane, and all the other logic is referenced to the digital ground plane? I plan to run the ADC outputs to a backplane tristate data bus which is going to be pretty noisy to begin with so I think I need all the noise margin I can get.
A. Well, nobody ever said life was easy or fair! You have reached the right conclusion by traveling a rocky road, but the problems you suggest-digital noise on your analog ground plane and reduced noise margin on your ADC outputs-really arent as bad as they seem; they can be overcome. It is clearly better to let a few hundred millivolts corrupt the digital interface than to apply the same corrupting signal to the analog input where the least-significant-bit for a 16-bit, 10-V-input-range ADC is only 150 µV! First of all, the digital ground currents on DGND pins cant really be that bad, or they would have degraded the internal analog parts of the ADC in the first place! If you bypass the power pins of the ADC to the analog ground plane, using a good-quality high-frequency ceramic capacitor for high frequency noise (say 0.1 µF), you will isolate these currents to a very small region around the IC, and they will have minimal effect on the rest of your system.
You will incur some reduction in digital noise margin, but it is usually acceptable with TTL or CMOS logic if its less than a few hundred millivolts or so. If your ADC has single-ended ECL outputs, you may want to put a push-pull gate on each digital output-i.e., one with both true and complementary outputs. Tie the grounds of this gate package to the analog ground plane and connect the logic signals differentially across the interface. Use a differential line receiver at the other end which is grounded to the digital ground plane. The noise between the analog and digital ground planes is now common-mode-most of it will be rejected at the output of the differential line receiver. You could use the same technique with TTL or CMOS, but there is usually enough noise margin not to require differential transmission techniques.
However, one thing you said troubles me greatly. In general, it is unwise to connect the ADC outputs directly to a noisy data bus. The bus noise may couple back into the ADC analog input through the stray internal capacitance-which may range from 0.1 to 0.5 pF. It is much better to connect the ADC outputs directly to an intermediate buffer latch located close to the ADC. The buffer latch is grounded to your digital ground plane, so its output logic levels are now compatible with those of the rest of your system.

Q. I think I understand now, but why on earth didnt you just call all the ground pins of your ADC AGND in the first place; then none of this would have come up in the first place?
A. Perhaps. But what if the incoming-inspection person connects an ohmmeter between these pins and finds out that they are not actually connected together inside the package? The whole lot will probably be rejected-and the IC may be blown! Furthermore, there is a tradition associated with ADC data sheets which says we must label the pins to indicate their true function, not what we would like them to be.
Q. O. K. Now, here comes a question Ive been saving as your ultimate test! I have a colleague who designed a system with separate analog and digital ground systems. My colleague says that, with the ADCs AGND pin connected to the analog ground plane and the DGND pin connected to the digital ground plane, the system is working fine! How do you explain this?
A. First of all, just because a practice is not recommended doesnt necessarily mean you cant get away with it some of the time and thereby be lulled into a false sense of security. (This is one of the lesser-known of Murphys Laws). Some ADCs are less sensitive to external noise between the AGND and DGND pins, and it may be that your colleague picked one of those by accident. There could be other explanations-which would require that we explore your colleagues definition of working fine-but the point is that the ADCs specifications are not guaranteed by the manufacturer under those operating conditions. With a complex component like an ADC, it is impossible to test the device under all possible operating circumstances, especially those which arent recommended in the first place! Your friend got lucky this time, but you can be sure that Murphys law will ultimately catch up with him (or her) if this practice is continued in future system designs.
Q. I think I understand the ADC grounding philosophy now, but what about DACs?
A. The same philosophy applies. The DACs AGND and DGND pins should be tied together and connected to the analog ground plane. If the DAC has no input latches, the registers driving the DAC should be referenced and grounded to the analog ground plane to prevent digital noise from coupling into the analog output.
Q. What about mixed-signal chips which contain ADCs, DACs, and DSPs such as your ADSP-21msp5O voiceband processor?
A. The same philosophy applies. You should never think of a complex mixed-signal chip, such as the ADSP-21msp50, as being only a digital chip! The same guidelines weve just been discussing should be applied. Even though the effective sampling rate of the 16-bit sigma-delta ADC and DAC is only 8 ksps, the converters operate at an oversampling frequency of 1 MHz. The device requires an external 13-MHz clock, and an internal 52- MHz processor clock is generated from it with a phase-locked loop. So you see, successful application of this device requires an understanding of design techniques for both precision- and high-speed circuits.
Q. What about the analog and digital power-supply requirements of these devices? Should I buy separate analog and digital power supplies or use the same supply?
A. This really depends on how much noise is on your digital supply. The ADSP-21msp50, for example, has separate pins for the +5- V analog supply and the +5-V digital supply. If you have a relatively quiet digital supply, you can probably get away with using it for the analog supply too. Be sure to properly decouple each supply pin at the device with a 0.1-µF ceramic capacitor. Remember to decouple to the analog ground plane, not the digital ground plane! You may also want to use ferrite beads for further isolation. The diagram below shows the proper arrangement. A much safer solution is to use a separate +5-V analog supply. You can generate the +5 V from a quiet +15-V or +12-V supply using a three-terminal regulator, if you can tolerate the extra power dissipation.

REFERENCES [not available from Analog Devices unless noted]
1. Ralph Morrison, Grounding and Shielding Techniques in Instrumentation, Third Edition. New York: Wiley-lnterscience, 1986.
2. Henry W. Ott, Noise Reduction Techniques in Electronic Systems, Second
Edition. New York: Wiley-Interscience, 1988.
3. High-Speed Design Seminar, 1996. Norwood MA: Analog Devices, Inc.
4. Mixed-Signal Design Seminar, 1991. Norwood MA: Analog Devices, Inc.
5. Paul Brokaw, An I.C. Amplifier Users Guide to Decoupling, Grounding
and Making Things Go Right for a Change. AN-202. Free from Analog Devices.
6. Jeff Barrow, Avoiding Ground Problems in High Speed Circuits, R.F.
Design, July, 1989.
7. Paul Brokaw and Jeff Barrow, Grounding for Low- and High-Frequency Circuits, Analog Dialogue 23-3, 1989. Free from Analog Devices.
8. The Best of Analog Dialogue-1967-1991. Norwood MA: Analog Devices, Inc. Free from Analog Devices.
ODDS N ENDS (Continued from earlier issues)
by James Bryant
TIME REFERENCES(continued from 26-1-AA-11)
Q. Why do you say that the clock of a system is a reference?
A. This comment does not necessarily apply to the conversion clock of an ADC; it applies principally to the sampling clock of a sampled-data system. In these systems, the signal is required to be sampled repeatedly at predictable (usually equal) intervals for storage, communication, computational analysis, or other types of processing. The quality of the sampling clock is a system-performance-limiting factor.
Q. But crystal oscillators are very stable, arent they?
A. They have good long-term stability, but they are often used in ways which introduce short-term phase noise. Phase noise is also introduced by designers who, instead of using crystal oscillators, use R-C relaxation oscillators (such as the 555 or the 4046)-which have a great deal of phase noise.
Q. How can I ensure that my sampling clock has low phase noise?
A. Dont use the crystal oscillator circuitry in your microprocessor or DSP processor as the source of your sampling clock. If at all possible, do not use a logic gate in a crystal oscillator. Crystal oscillators made with logic gates generally overdrive the crystal; this is bad for its long term stability, and usually introduces worse phase noise than would a simple transistor oscillator. In addition, digital noise from the processor-or from other gates in the package if a logic gate is used as an oscillator-will appear as phase noise on the oscillator output.
Q. But crystal oscillators are very stable, arent they?
A. Ideally, use a single transistor or FET as your crystal oscillator and buffer it with a logic gate. This logic gate, and the oscillator itself, should have a well-decoupled supply; the other gates in the package should not be used because logic noise from them will phase-modulate the signal. (They may be used for dc applications but not for fast-switching operations.)
If there is a divider between the crystal oscillator and the sampling clock input of the various ADCs, the divider power supply should be decoupled separately from the system logic to keep power supply noise from phase-modulating the clock.
The sampling clock line should be kept away from all logic signals to prevent pickup from introducing phase noise. Equally, it should be kept away from low-level analog signals lest it corrupt them.
Q. You have told me not to use the clock oscillator of my processor as the sampling clock source. Why not? Isnt it sensible to use the same oscillator for both, since there will then be a constant phase relationship between the signals?
A. True. But in such cases, it is often better to use a single discrete low-noise oscillator to drive the processor clock input and the sampling clock divider through separate buffers (though they may share a package) than to use the oscillator in the processor. In medium-accuracy systems with low sampling rates it may be possible to use the processors internal oscillator-but check with the diagram below).
Q. Just how serious is this problem of noise on a sampling clock? I hardly ever see it mentioned in articles on sampled data systems.
A. The phase noise of the sampling clock is often ignored, because the limiting factor on system performance used to be the aperture jitter of the of the sample-hold-but if we consider the system as a whole, aperture jitter is just one component of the total phase noise in the sampling clock chain. With modern sampling ADCs the aperture jitter may be less important than other components of phase noise.

The diagram shows the effect of the total phase jitter of the sampling clock on signal-to-noise ratio (SNR) or effective number of bits (ENOB). This jitter has the rms value of tph, which is made up of the root-sum-of-squares of the phase jitter on the sampling clock oscillator, the phase jitter introduced by pickup during transmission of the sampling clock through the system, and the aperture jitter of the SHA in the sampling ADC. This diagram may be somewhat unsettling, as it shows just how little phase noise is required to corrupt a high-resolution sampled-data system.
MORE ON TRIMMING
Q. I dont have enough range to adjust the offset of my circuit-and it seems to have rather more drift than Id expected.
A. Ill bet the amplifier is a bipolar type and you are using its offset-trim terminals to trim other circuit voltages.
Q. How did you guess?
A. The range of offset adjustment of an op amp is normally 2 to 5 times the maximum expected offset of the lowest grade of the device (in some early op amps, it was much larger, but such a wide range is not ideal). If the lowest grade has a VOS (max) of ±1 mV, then the likely adjustment range with the recommended circuit is ±2 to ±5 mV.
If the external voltage you are attempting to compensate for is larger than this (referred to the op amps input), you will not be able to do so with the amplifiers offset-trim terminals.
Furthermore, if you are using a bipolar-input op amp, it is inadvisable to use these terminals for external offset correction because drift will be increased. Heres why: the input stage thermal drift is proportional to the internal offset; if this
has been trimmed to a minimum, the drift will also be a minimum. If you then trim the amplifier to compensate for an external offset, drift will no longer be minimized. However, FET-input op amps have separately trimmed offset and drift, their offset adjustment terminals may thus be used for small system adjustments.
|