|
「アナログ・デバイセズに寄せられた珍問/難問集より」のRAQコラム、が米国のEDNとDesign Newsで毎月刊行されます。 アナログ・デバイセズのエキスパートが課題を解決する、技術的なトラブルシューティング、見識やアイデア等をご紹介します。
|
|
Questions & Answers
奇妙だけど本当にあった珍問/難問集
| Issue 50: | What's the big deal about ABSOLUTE MAXIMUM RATINGS? |
The Question: Is it alright to exceed just one of the parameters in the ABSOLUTE MAXIMUM RATINGS table, by just a little bit? Download this article [pdf, 102,089 bytes] |
| Issue 49: | What's the (Converter) Frequency Kenneth? |
The Question: How Do I Design a Converter Front-end without Compromising the Performance? Download this article [pdf, 97,703 bytes] |
| Issue 48: | Some Chips Have Moving Parts! |
The Question: Is it true that over the years electrical devices have evolved to where they have no moving parts at all? Download this article [pdf, 104,025 bytes] |
| Issue 47: | Which carries more weight, a datasheet or SPICE macromodel? |
The Question: When running a SPICE (Simulation Program with Integrated Circuit Emphasis) simulation with one of your amplifier models, I get different results than those shown in the datasheet. Which should I believe? Download this article [pdf, 100,637 bytes] |
| Issue 46: | What shall we do with an unused op-amp? |
The Question: In the RAQ on op-amps as comparators you mentioned an unused op-amp in a quad as being possible justification for using it as a comparator. What do you do if you've an unused op-amp and don't need a comparator? Download this article [pdf, 129,560 bytes] |
| Issue 45: | Glass Diodes May See the Light and Hum |
The Question: A few months ago you discussed how to prevent the inherent high frequency (HF) noise of a switching supply from escaping into sensitive analog circuits and corrupting them. My op-amp output hums and no amount of supply filtering helps. What should I do? Download this article [pdf, 127,971 bytes] |
| Issue 44: | Keeping Common Modes Common |
The Question: How come my A/D converter is not able to achieve full scale as the datasheet specifies? Download this article [pdf, 95,957 bytes] |
| Issue 43: | Impedance Measuring Chip Offers
Little Resistance to Applications |
The Question: I came across your Impedance measuring chip (IMC) in a recent article. It sounds interesting, but how does it work and what can it be used for? Download this article [pdf, 125,661 bytes] |
| Issue 42: | Are Your Filters Filtering? |
The Question: Why is my A/D converter's anti-aliasing filter showing inadequate spurious and noise rejection? Download this article [pdf, 731,084 bytes] |
| Issue 41: | What's in Your Toolbox? |
The Question: Do you prefer power tools or hand tools for solving problems? Download this article [pdf, 103,363 bytes] |
| Issue 40: | How Big Is It? |
The Question: How can I handle signals with huge variations in amplitude? Download this article [pdf, 102,537 bytes] |
| Issue 39: | Off-amps, what the heck are off-amps? Op amps with no power applied, of course. |
The Question: What kind of performance (pick a parameter, it could be input impedance or any other op amp specification) can I expect from your amplifier ... when the power is off? Download this article [pdf, 126,118 bytes] |
| Issue 38: | Single Supply Amplifiers They Sound Simple ... are they? |
The Question: Running rail-to-rail op amps on a single supply sounds like a winning combination, but what drawbacks will I encounter when using amplifiers like this? Download this article [pdf, 119,519 bytes] |
| Issue 37: | Lock Down That Noise - Don't Let It Escape |
The Question: How can I prevent switching-mode power supply noise from devastating my circuit performance? Download this article [pdf, 1,056,768 bytes] |
| Issue 36: | The Difference Between Different Differential Amplifiers |
The Question: I'm perplexed. Why is the output voltage of my ADC differential amplifier driver not what it should be? Download this article [pdf, 737,280 bytes] |
| Issue 35: | Stress Is Bad For You and For Analog ICs
|
The Question: Does too much mechanical stress when mounting precision analog ICs damage their accuracy? Download this article [pdf, 126,976 bytes] |
| Issue 34: | 容量切除術ですって? ものすごく痛そう! |
質問: 高速トリプル・アンプの1つが発振します。どこが悪いのでしょうか? この記事をダウンロードする [pdf, 510,034 bytes] |
| Issue 33: | ヒステリシスは魔法を阻止する |
質問: 高精度アナログ回路を再キャリブレーションすれば、精度が高くなるでしょうか? この記事をダウンロードする [pdf, 746,811 bytes] |
| Issue 32: | 政治的公正とデータシート |
質問: データシートの仕様:癪の種か混乱の種か? この記事をダウンロードする [pdf, 502,404 bytes] |
| Issue 31: | 熱すぎるのも冷たすぎるのも、ちょうどいいのかもしれない |
質問: 絶対最大温度と絶対最小温度は、電圧定格や電流定格と同じように絶対なのでしょうか? この記事をダウンロードする [pdf, 1,147,715 bytes] |
| Issue 30: | 容量センサー:実際に使えるほど堅牢なのか? |
質問: 容量センサーが民生用電子機器で使用されているのは知っていますが、過酷な工業環境で使えるほど堅牢でしょうか? この記事をダウンロードする [pdf, 866,267 bytes] |
| Issue 29: | 半分あるのか、半分空なのか?容量についてのさまざまな考え方 |
質問: 2本のワイヤを持ったすべてのコンポーネントは、以前話題になった抵抗と同じくらい複雑なのでしょうか? この記事をダウンロードする [pdf, 766,410 bytes] |
| Issue 28: | 電気によるアンプの発熱はどんな具合か?(あるいは正確な温度測定とは…すべて程度の問題である) |
質問: 小型パッケージのオペアンプや類似のデバイスのダイ温度を測定する一番良い方法は何でしょうか? この記事をダウンロードする [pdf, 742,779 bytes] |
| Issue 27: |
抵抗(と老婦人)には秘められた深みがある |
質問: 以前、抵抗の熱ノイズについて説明していただきました。抵抗は、接続端が2つだけ、抵抗値という単純な特性が1つだけのきわめて簡単なコンポーネントに思われます。こんなものでも、うっかりとはまってしまう罠がまだ他にもあるのでしょうか? この記事をダウンロードする [pdf, 1,121,369 bytes] |
| Issue 26: |
オペアンプのノイズにも耳をつんざくようなものがある
|
質問: 前回、オペアンプのノイズを外部抵抗のせいにされました。いつもそうとは限らないと思うのですが、いかがでしょうか? この記事をダウンロードする [pdf, 1,292,170 bytes] |
| Issue 25: |
抵抗ノイズが耳をつんざくような大きさで、小さくできない |
質問: 私の低ノイズ・アンプはあまり低ノイズではありません。どこか間違えているのでしょうか? この記事をダウンロードする [pdf, 838,115 bytes] |
| Issue 24: |
アンプの配管101:リーク(漏れ)の多いアンプは設計を台無しにするか?
|
質問: 電源オフの状態にも関わらず、アンプの出力が低レベルの信号をリークします。なぜでしょう…この回路は駄目なのでしょうか? この記事をダウンロードする [pdf, 1,279,071 bytes] |
| Issue 23: |
回路を壊すのと、試験装置を壊すのとどちらがいいか?有能なエンジニアなら、自分の設計だけでなく、あらゆることに疑問を抱き、変更を試みることが必要となります。 |
質問: 新しい高速アンプ・ボードをプローブしていたら、出力に大きなオーバーシュートが発生しており、まるでベルみたいにリンギングしていることに気がつきました。レイアウト、電源バイパスの最適化、グラウンディング、寄生リアクタンス、パターン終端には十分に注意したのですが。いったいどこがいけなかったのでしょう? この記事をダウンロードする [pdf, 1,279,071 bytes] |
| Issue 22: |
ものごと(動物とADC)は必ずしも見かけどおりとは限らない
|
質問: 低速のADC を駆動するとき、高周波問題を考慮する必要はあるでしょうか? この記事をダウンロードする [pdf, 4,679,083 bytes] |
| Issue 21: |
表面実装ICのブレッドボーディング、小さすぎるか、小さすぎないか?それが問題だ…
|
質問: 超小型の表面実装(SM)ICを使ったブレッドボードを作成するにはどうすればよいのでしょうか? この記事をダウンロードする [pdf, 450,815 bytes] |
| Issue 20: |
イゴール、私に電源シーケンサを渡してくれ!
|
質問: 先月、絶対最大定格には集積回路(IC)の他のピンの値に依存する場合があると言われました。パワーアップ時にそのような絶対最大定格を超えないようにするにはどうしたらよいのでしょうか? この記事をダウンロードする [pdf, 1,221,948 bytes] |
| Issue 19: |
最大定格の遵守、あるいは不幸な予言を避ける方法
|
質問: 「絶対最大」定格にはどれぐらいの安全マージンがあるのでしょうか? この記事をダウンロードする [pdf, 1,154,701 bytes] |
| Issue 18: |
いったいウィリアム・テルはどの程度正確だったのか?
|
質問: A/D コンバータ(ADC)はどの程度正確でしょうか? この記事をダウンロードする [pdf, 1,324,777 bytes] |
| Issue 17: |
チップは多いほうがいいということ(あるいはベルギーの食べ物の優れている点)
|
質問: チップが1つよりも2つのほうがいいのはどんな場合ですか? この記事をダウンロードする [pdf, 6,200,025 bytes] |
| Issue 16: |
フォトカプラをデジタル・アイソレータに置き換えること(あるいは真夜中の騎行をどのように回避できたか)
|
質問: トランス・ベースのアイソレータをフォトカプラの代わりにすることができるでしょうか?DC信号、磁界、サイズに問題が生じないでしょうか? この記事をダウンロードする [pdf, 1,157,866 bytes] |
| Issue 15: |
高精度アナログICの長期安定性、
あるいは優雅に年をとって突然死を避ける方法
|
質問: 私の製品の平均寿命は20年です。製品のキャリブレーションは どれぐらい長持ちするのでしょうか? この記事をダウンロードする [pdf, 1,118,120 bytes] |
| Issue 14: |
創意工夫に富んでいること、あるいは優れたエンジニア(および優れた料理人)が手に入る中で最上のコンポーネント(材料)を使用する理由
|
質問: 携帯電話/歪みゲージ/医療用超音波機器システムにはどんなアンプ/スイッチ/コンバータが最適でしょうか? この記事をダウンロードする [pdf, 1,060,347 bytes] |
| Issue 13: |
チンプンカンプンと思われるかもしれませんが、ΣΔコンバータはそれほど難しいものではありません
|
質問: ΣΔコンバータの仕組みを、クマのプーさん(頭の足りないクマさん)でもわかるように簡単に説明していただけますか? この記事をダウンロードする [pdf, 1,308,655 bytes] |
| Issue 12: | アクティブ・フィルタを設計しない方法(あるいはダイバーの気を散らすのはサメだけではない) |
質問: アクティブ・フィルタを入念に設計したのに仕様に合わないのはなぜでしょうか? この記事をダウンロードする [pdf, 1,053,103 bytes] |
| Issue 11: |
コンパレータとオペアンプ ― ともに相交わることなかれ(あるいはパンチ君からのアドバイス) |
質問: オペアンプで間に合うのに、なぜ高価なコンパレータを買うのでしょうか? この記事をダウンロードする [pdf, 961,745 bytes] |
| Issue 10: | デジタル処理は必ずしも万能ではない
(あるいは何がアナログ・エンジニアを笑わせたのか)
|
質問: デジタル・システムの方が安くて強力なのに、なぜアナログ信号処理 を推奨するのでしょうか? この記事をダウンロードする [pdf, 962,470 bytes] |
| Issue 9: | コンバータの接地(あるいは救いの哲学!)
|
質問: 最近、ADCのデジタル・グラウンド・ピンをシステムのアナログ・グラウンドに接続するようにアドバイスされましたが、信じられません。間違いではありませんか? この記事をダウンロードする [pdf, 1,124,582 bytes] |
| Issue 8: | グランド・ノイズとグランドホッグ - 電子技術者たちの民間伝承
|
質問: アナログ入力がグランディング(接地)されているのに、なぜ出力でもグランドが必要なのでしょうか? この記事をダウンロードする [pdf, 6,638,459 bytes] |
| Issue 7: | エンジニアに酒を飲ませるのは簡単だが、詩に興味を持たせるには? |
質問: SPICEシミュレーションは完璧だったのに、量産バッチになると仕様に適合しません。 この記事をダウンロードする [pdf, 1,062,670 bytes] |
| Issue 6: |
チックタック、チックタック
|
質問: 私のクロックの精度を1ppmにしたいのですが ― どうすれば精度を上げられますか? この記事をダウンロードする [pdf, 1,368,806 bytes] |
| Issue 5: | バイアス電流のチェック(あるいは神様からの祝福の言葉を聞いてもらう方法) |
質問: 日のオペアンプのバイアス電流は非常に小さくなっていますが、気にする必要はありますか? この記事をダウンロードする [pdf, 438,878 bytes] |
| Issue 4: | 買主の危険負担に気をつけて! |
質問: データシートはどうやって理解したらいいのでしょうか? この記事をダウンロードする [pdf, 1,098,362 bytes] |
| Issue 3: | 重要なディテールの分離(あるいは人魚と酢漬けのニシンの昼食) |
質問: 私のCMOSマルチプレクサには問題があるのでしょうか? この記事をダウンロードする [pdf, 1,246,924 bytes] |
| Issue 2: | スロースタートのA/D コンバータ(あるいはコンバータの問題の診断における有益な効果) |
質問: 節電のため、私のA/D コンバータ(ADC)は測定のときだけ起動するようにしています。連続動作ではシステムは非常に正確なのに、電源を入れたり、切ったりすると全く予測不可能になってしまいます。 この記事をダウンロードする [pdf, 6,459,229 bytes] |
| Issue 1: | 無線周波数干渉(あるいは高級レストランで昼食をご馳走になる方法) |
質問: RF(無線周波数)は低周波回路に異常を招くことがあると聞きましたが、どういうことでしょうか? この記事をダウンロードする [pdf, 6,584,970 bytes] |