CN0122: High Speed Instrumentation Amplifier Using the AD8271 Difference Amplifier and the ADA4627-1 JFET Input Op Amp

Engineered. Tested. Ready to Integrate.詳細をみる

回路の説明

回路の機能とその利点
  • High speed instrumentation amplifier design
  • Great common mode rejection ratio
使用されている製品
    アプリケーション: 
  • センサー/センサー インターフェース
  • 電子試験&測定

CIRCUIT FUNCTION AND BENEFITS

A traditional method for building an instrumentation amplifier is to use three op amps and seven resistors as shown in Figure 1. This approach requires four precision matched resistors for a good common-mode rejection ratio (CMRR). Errors in matching will produce errors at the final output. An imbalance of one or two picofarads on certain nodes will drastically degrade the high frequency CMRR, a fact often overlooked.

This circuit uses a monolithic difference amplifier with laser trimmed thin film resistors for the output amplifier, thereby providing good dc and ac accuracy with fewer components than the traditional approach.

Figure 1. In Amp with Gain = 201 (Simplified Schematic: Decoupling and All Connections Not Shown)

CIRCUIT DESCRIPTION

This circuit utilizes the AD8271 difference amplifier and two ADA4627-1 amplifiers, which have low noise, low drift, low offset, and high speed. For high impedance sources, the ADA4627-1 is an ideal choice for the input stage amplifiers due to the extremely low input bias current of their JFET inputs.

The op amps selected for the input stage must also have low offset voltage and low offset voltage drift with temperature. They also need to have good drive characteristics. This allows the use of low value resistors to minimize resistor thermal noise.

Headroom issues relating to the op amp must be considered in this circuit for proper operation.

When working with any op amp having a gain-bandwidth product greater than a few MHz, careful layout and bypassing are essential. A typical decoupling network consists of a 1 μF to 10 μF electrolytic capacitor in parallel with a 0.01 μF to 0.1 μF low inductance ceramic MLCC type.

For the lowest noise with low impedance sources only, low voltage noise is important. The AD8599 has lower noise, lower offset voltage drift, and lower supply current; but the input bias currents are much higher, and the bandwidth will be lower than that obtained with the ADA4627-1. The measured −3 dB points are 56.6 kHz and 87.6 kHz for the AD8599 and ADA4627-1, respectively. (See Figure 2).

Figure 2. Bandwidth of Circuit Shown in Figure 1 Comparing the ADA4627-1 to the AD8599 as the Input Stage.

With high impedance sources, the input bias current and the input noise current of a bipolar op amp can result in errors. The bias current creates an I × R drop, which will be multiplied by the overall circuit gain. This can result in several volts of offset at the output. The input noise current is also multiplied by the source impedances, creating an additional noise voltage. To avoid this, a JFET input op amp, such as the ADA4627-1, should be used. Even though the voltage noise is slightly higher than the AD8599, the current noise is significantly lower, resulting in lower overall noise when used with high impedance sources.

As Figure 3 and Figure 4 show, the AD8599 is the proper choice with low source impedances, and the ADA4627-1 is better with higher source impedances. There is a trade-off: the input capacitance of JFET op amps is higher than bipolar op amps, so the RC time constant must be considered.

Figure 3. Noise Spectral Density (RTO) of Circuit Shown in Figure 1 Comparing the ADA4627-1 to the AD8599 as the Input Stage: Low Impedance Source (0 Ω)
Figure 4. Noise Spectral Density (RTO) of Circuit Shown in Figure 1 Comparing the ADA4627-1 to the AD8599 as the Input Stage: High Impedance Source (66 kΩ)

COMMON VARIATIONS

The AD8271 or AD8274 can be used with a variety of op amps to optimize the overall performance with respect to supply current, signal bandwidth, temperature drift, and noise.

For the lowest possible drift over temperature, one of the auto-zero amplifiers, such as the AD8539, can be used, but the bandwidth will be reduced and wideband noise increased. This would be an excellent choice for bandwidths less than 10 Hz, however.

When selecting op amp and difference amplifier combinations for this circuit, always ensure that the input common-mode voltage range of each amplifier is not violated. This is commonly overlooked but is the subject of a fair number of application questions.

If the first stage gain is greater than about five, consider using a decompensated op amp, such as the OP37, to get a higher slew rate and signal bandwidth with less supply current. To avoid common- mode oscillation, the circuit must be modified slightly as described in "Phase Compensation of the Three Op Amp Instrumentation Amplifier." White, D. Rod. IEEE Transactions on Instrumentation and Measurement. Vol. IM-36, No. 3, Sept. 1987.

With microvolt-level input signals and a gain of 1000, the first stage can be operated on ±2.5 V, saving power and giving more choices of op amps, such as the AD8539 auto-zero amplifier. However, if the input common-mode voltage range is high, an op amp with a higher supply voltage must be chosen for the first stage.

この回路に使用されている製品&サンプル:

製品 概要 サンプルが入手可能な製品
AD8271 デファレンス・アンプ、プログラマブル・ゲイン、高精度 AD8271ARMZ AD8271BRMZ
AD8274 ディファレンス・アンプ、高精度、超低歪み AD8274ARMZ AD8274ARZ
AD8599 オペアンプ、デュアル、超低歪み、超低ノイズ AD8599ARZ
ADA4627-1 オペアンプ、JFET入力段、36V、19MHz、低ノイズ、低入力バイアス電流 ADA4627-1BRZ ADA4627-1ARZ ADA4627-1ACPZ-R7
沪ICP备09046653号
この回路へのコメントを送る X
content here.
content here.

この回路へのコメントを送る

閉じる