Analog Devices Technical Bookstore
Now available, a series of ADI Technical books covering a wide range design topics, from Practical Analog Techniques to Mixed Signal and DSP information. These books have been written by the Applications Engineering Staff at Analog Devices, including well-known authors such as Walt Kester, Walt Jung, James Bryant and Hank Zumbahlen. Books are priced at $40.00 each.
Also available at no cost is the third edition of "A Designer's Guide to Instrumentation Amplifiers" by Charles Kitchin and Lew Counts.
To purchase one of the books (or to order a free copy of "A Designer's Guide to Instrumentation Amplifiers"), click on the links below.
Basic Linear Design
Effective analog circuit design requires a strong understanding of linear devices. Linear Circuit Design Handbook bridges the gap between component theory and practical circuit design. Providing complete coverage of analog components and showing how to use them effectively, it serves as a useful reference for engineers involved in analog and mixed-signal design.
計装アンプの設計ガイド 完全版 (zip, 5,435 KB) Download Now (FREE!)
「計装アンプ」については、正しく理解されていない場合があります。計装アプリケーションで使用されるアンプがすべて計装アンプとは限りません。また、計装アンプのすべてが計装アプリケーションにのみ使用されるわけではありません。計装アンプは、モータ制御からデータ・アクイジション、車載機器にいたるまで、さまざまなアプリケーションで使用されています。この設計ガイドでは、計装アンプの基礎、動作原理、使用方法と用途について説明します。また、さまざまな種類の計装アンプについても取り上げています。
Analog-Digital Conversion Order Now ($40)
Analog-Digital Conversion presents a comprehensive set of notes presented in a recent Analog Devices seminar series on data converters. In a digital world, A/D and D/A conversion is essential to translate between analog real-world physical variables and the abstract 1s and 0s of digital processing. The book offers a hint of its breadth, as well as its orientation to practical design: Data-converter history; Fundamentals of sampled-data systems; Data-converter architectures; Data-converter process technology; Testing data converters; Interfacing to data converters; Data-converter support circuits; Data-converter applications; and Hardware design techniques.
High-Speed Design Techniques Order Now ($40)
The book, High Speed Design Techniques, contains chapters on high speed operational amplifiers, RF/IF subsystems, high speed sampling and high speed A/D Converters, high speed D/A converters and DDS systems. It also covers high speed hardware design techniques.
Mixed Signal and DSP Design Techniques Order Now ($40)
This book covers sampled data systems, choosing A-to-D and D-to-A converters for DSP applications, fast Fourier transforms, digital filters, selecting DSP hardware, interfacing to DSP chips, and hardware design techniques. This book explains signal processing hardwarehow it works, how to interface to it, and how to design it and debug it. Master the art and science of mixed-signal and DSP design with this informative and practical guide.