-
Products
- Amplifiers and Comparators
- Analog Microcontrollers
- Analog to Digital Converters
- Audio/Video Products
- Broadband Products
- Clock and Timing
- Digital to Analog Converters
- Embedded Processing and DSP
- Fiber/Optic
- Interface
- MEMS
- Power Management
- References
- RF/IF Components
- Sensors
- Switches/Multiplexers
- Temperature Sensing and Thermal Management
- Other Products
- Analog/HDMI/DVI Interfaces
- Audio A/D Converters
- Audio Amplifiers
- Audio CODECs
- Audio D/A Converters
- Audio Signal Processors
- Camera/Camcorder Analog Front Ends
- Display Driver Electronics
- iMEMS® Microphone
- Lens Driver Components
- Mobile TV Tuners
- Sample Rate Converters
- Video Amps/Buffers/Filters
- Video CODECs
- Video Compression
- Video Decoders
- Video Encoders
OTHERS WAYS
TO FIND PRODUCTSSelection Guides Product Selection Tables - Resources & Tools
-
About ADI
- My Analog
ADI engineers share their lab work with you in this
‘Circuits from the Lab’ Circuit Note.
You can combine these product pairings quickly and with confidence.
Please review our Circuits from the Lab Information and Disclaimer page
for more details.
CN0060
ADI engineers share their lab work with you in this ‘Circuits from the Lab’ Circuit Note. You can combine these product pairings quickly and with confidence. Please review the disclaimer at the bottom of the page for more information.
Copyright 2008, Analog Devices, Inc. All rights reserved. "Circuits from the Lab" from Analog Devices have been designed and built by Analog Devices engineers. Standard engineering practices have been employed in the design and construction of each circuit, and their function and performance have been tested and verified in a lab environment at room temperature. However, you are solely responsible for testing the circuit and determining its suitability and applicability for your use and application. Accordingly, in no event shall Analog Devices be liable for direct, indirect, special, incidental, consequential or punitive damages due to any cause whatsoever connected to the use of any "Circuits from the Lab". Circuit variations described in the Common Variations section of the document have not necessarily also been built and tested.
"Circuits from the Lab" are intended only for use with Analog Devices products and are the intellectual property of Analog Devices or its licensors. While you may use the "Circuits from the Lab" in the design of your product, no other license is granted by implication or otherwise under any patents or other intellectual property by application or use of the "Circuits from the Lab". Information furnished by Analog Devices is believed to be accurate and reliable. However, "Circuits from the Lab" are supplied "as is" and without warranties of any kind, express, implied, or statutory including, but not limited to, any implied warranty of merchantability, noninfringement or fitness for a particular purpose and no responsibility is assumed by Analog Devices for their use, nor for any infringements of patents or other rights of third parties that may result from their use. Analog Devices reserves the right to change any "Circuits from the Lab" at any time without notice, but is under no obligation to do so. Trademarks and registered trademarks are the property of their respective owners.
Low Cost Differential Video Receiver Using the ADA4851 Amplifier and the ADV7180 Video Decoder
  (CN0060)| Circuit Types: | ADC Circuit/Driver |
| Optimized For: | High Performance, High Speed |
| Applications: | Audio / Video, Automotive |
The circuit described in this document and shown in Figure 1 provides a low cost, low power, unipolar, differential receiver using the ADA4851-1 for an incoming video signal before being digitized by the ADV7180 video decoder. This circuit eliminates common mode noise and phase noise caused by ground potential difference from an incoming video signal and is well suited for automotive infotainment and vision safety systems. The ADA4851 family of amplifiers along with the ADV7180 video decoder are all AECQ100 qualified which makes both products ideal for automotive applications.
Low power, low cost, high speed and fast settling make these amplifiers well suited for many video applications where these requirements are very important. Figure 1 only shows a single amplifier for simplicity, the amplifier circuit can be copied for each input for as many times as needed.
The ADA4851-1 is a single (also available as a dual or quad amplifier in a single package) 130MHz, low power, low cost, high speed, voltage feedback, rail-to-rail output amplifier that has an operating supply range of +3 V to +5 V. In Figure 1 the ADA4851-1 is configured as a low cost differential to single-ended receiver for video signals. This configuration is a standard 4-resistor difference amplifier optimized for composite video frequencies, with a differential to single-ended gain of 1. The amplifier only amplifies the difference between the two inputs while eliminating the common mode noise between the incoming signals and allowing the reconstruction of the original signal. Using low value, high accuracy resistors and a high CMRR amplifier provides the exceptional performance.
A critical design consideration that is important to note about this architecture is its dependence on resistor matching for the Common Mode Rejection (CMR) of this circuit design. The CMR can be calculated using the following formula.

In this expression, the term “Kr” is a single resistor tolerance in fractional form (1% = 0.01 etc), and it is assumed that the amplifier has significantly higher CMR performance. Using this formula, it shows that if 54dB or better CMR is desired, then R1, R2, R3 and R4 need to have a matching tolerance of 0.1% or better.
To prevent the incoming signal from violating the input and output voltage range, it is necessary to add a DC offset. This is conveniently done by connecting R4 to the 1.8V analog supply voltage (AVDD 1.8V) also used by the ADV7180, which helps in keeping the cost low. To prevent supply noise from coupling into the video signal stream, be sure to have adequate bypassing on this supply (AVDD 1.8V) as shown in Figure 1.
Some automotive applications require AC-coupled inputs to protect the input to the amplifier from a short to a voltage higher than its supply voltage. The input impedance of 1 kΩ (R2 and R3) with the 22 μF capacitors (C1 and C2) sets a high pass corner frequency pole at approximately 7Hz. If a lower frequency is desired, increasing the capacitor value decreases the corner frequency proportionally. For example, using 47 μF capacitors results in a 3.4 Hz high pass corner frequency.
The ADV7180 automatically detects and converts standard analog baseband television signals compatible with worldwide NSTC, PAL, and SECAM standards into 4:2:2 component video data compatible with the 8-bit ITUR. 656 interface standards. The accurate 10-bit analog to digital conversion provides professional quality video performance for consumer applications with true 8-bit data resolution. Three analog video input channels accept standard composite, S-video, or component video signals, supporting a wide range of consumer video sources. AGC and clamp-restore circuitry allow an input video signal peak-to-peak range of up to 1.0 V.
There are a few options for supplying the DC bias voltage for the ADA4851. The ADR12X family of voltage references has a wide range of values that can be used. Another method is to add one more resistor that would form a voltage divider in conjunction with R4. Be sure that the parallel combination of R4 and the new R5 matches the value of Rf feedback resistor.
If better CMR performance and high input impedance is desired, the ADA4851 can be replaced with the AD8130.
Contributed February, 2009
On This Page:
Ask the Experts/Provide Feedback
Have questions
about this circuit or your upcoming design? Please contact
our experienced applications engineers who are readily available to assist you.
Have feedback on this circuit? Please provide it
here.
-
ADA4851-1:
Low Cost, High Speed, Rail-to-Rail, Output Op Amp (Single)The ADA4851-1 (single), ADA4851-2 (dual), and ADA4851-4 (quad) are low cost, high speed, voltage feedback rail-to-rail output op amps. Despite their low price, these parts provide excellent overall performance and versatility. The 130 MHz, −3 dB bandwidth and high slew rate make these amplifiers well suited for many general-purpose, high speed applications.
The ADA4851 family is designed More
Data Sheet Rev G, 09/2009 (pdf 480kB)
Data Sheet Rev G, 09/2009 (pdf 480kB) -
ADV7180:
10-Bit, 4× Oversampling SDTV Video DecoderThe ADV7180 automatically detects and converts standard analog baseband television signals compatible with worldwide NTSC, PAL, and SECAM standards into 4:2:2 component video data compatible with the 8-bit ITU-R BT.656 interface standard.
The simple digital output interface connects gluelessly to a wide range of MPEG encoders, codecs, mobile video processors, and Analog Devices, Inc., More
Data Sheet Rev D, 06/2009 (pdf 1290kB)
Data Sheet Rev D, 06/2009 (pdf 1290kB)
Evaluation Boards
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- ADV7180 Evaluation Board
- Universal High Speed Op Amp Evaluation Boards The Universal Evaluation Board allows the user to quickly and easily evalua...
- ADIsimOpAmp™ This tool will help with the selection, evaluation and troubleshooting of v...
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- ADA4851-1 SPICE Macro-Model
- ADV7180 IBIS Models