-
Products
- Amplifiers and Comparators
- Analog Microcontrollers
- Analog to Digital Converters
- Audio/Video Products
- Broadband Products
- Clock and Timing
- Digital to Analog Converters
- Embedded Processing and DSP
- Fiber/Optic
- Interface
- MEMS
- Power Management
- References
- RF/IF Components
- Sensors
- Switches/Multiplexers
- Temperature Sensing and Thermal Management
- Other Products
- Analog/HDMI/DVI Interfaces
- Audio A/D Converters
- Audio Amplifiers
- Audio CODECs
- Audio D/A Converters
- Audio Signal Processors
- Camera/Camcorder Analog Front Ends
- Display Driver Electronics
- iMEMS® Microphone
- Lens Driver Components
- Mobile TV Tuners
- Sample Rate Converters
- Video Amps/Buffers/Filters
- Video CODECs
- Video Compression
- Video Decoders
- Video Encoders
OTHERS WAYS
TO FIND PRODUCTSSelection Guides Product Selection Tables - Resources & Tools
-
About ADI
- My Analog
ADI engineers share their lab work with you in this
‘Circuits from the Lab’ Circuit Note.
You can combine these product pairings quickly and with confidence.
Please review our Circuits from the Lab Information and Disclaimer page
for more details.
CN0050
ADI engineers share their lab work with you in this ‘Circuits from the Lab’ Circuit Note. You can combine these product pairings quickly and with confidence. Please review the disclaimer at the bottom of the page for more information.
Copyright 2008, Analog Devices, Inc. All rights reserved. "Circuits from the Lab" from Analog Devices have been designed and built by Analog Devices engineers. Standard engineering practices have been employed in the design and construction of each circuit, and their function and performance have been tested and verified in a lab environment at room temperature. However, you are solely responsible for testing the circuit and determining its suitability and applicability for your use and application. Accordingly, in no event shall Analog Devices be liable for direct, indirect, special, incidental, consequential or punitive damages due to any cause whatsoever connected to the use of any "Circuits from the Lab". Circuit variations described in the Common Variations section of the document have not necessarily also been built and tested.
"Circuits from the Lab" are intended only for use with Analog Devices products and are the intellectual property of Analog Devices or its licensors. While you may use the "Circuits from the Lab" in the design of your product, no other license is granted by implication or otherwise under any patents or other intellectual property by application or use of the "Circuits from the Lab". Information furnished by Analog Devices is believed to be accurate and reliable. However, "Circuits from the Lab" are supplied "as is" and without warranties of any kind, express, implied, or statutory including, but not limited to, any implied warranty of merchantability, noninfringement or fitness for a particular purpose and no responsibility is assumed by Analog Devices for their use, nor for any infringements of patents or other rights of third parties that may result from their use. Analog Devices reserves the right to change any "Circuits from the Lab" at any time without notice, but is under no obligation to do so. Trademarks and registered trademarks are the property of their respective owners.
| Circuit Types: | RF/IF Driver |
| Optimized For: | High Performance, High Speed |
| Applications: | Communications, General Purpose |
The circuit described in this document provides closed-loop, automatic power control using a VGA (ADL5330) and a log detector (AD8318). Due to the high temperature stability of the AD8318, this circuit provides stability over temperature as the AD8318 RF detector ensures the same level of temperature stability at the output of the ADL5330 VGA. The addition of the log amp detector converts the ADL5330 from an open-loop variable gain amplifier into a closed-loop output power control circuit. Since the AD8318, like the ADL5330, has a linear-in-dB transfer function, the Pout vs. setpoint transfer function also follows a linear-in-dB characteristic.
Although the ADL5330 variable gain amplifier provides accurate gain control, precise regulation of output power can be achieved with an automatic gain control (AGC) loop. Figure 1 shows the ADL5330 operating in an AGC loop. The addition of the AD8318 log amp allows the AGC to have improved temperature stability over a wide output power control range
To operate the ADL5330 VGA in an AGC loop, a sample of the output RF must be fed back to the detector (typically using a directional coupler and additional attenuation). A set-point voltage is applied by a DAC to the VSET input of the detector while VOUT is connected to the GAIN pin of the ADL5330. Based on the detector’s defined linear-in-dB relationship between VOUT and the RF input signal, the detector adjusts the voltage on the GAIN pin (the detector’s VOUT pin is an error amplifier output) until the level at the RF input corresponds to the applied setpoint voltage. GAIN settles to a value that results in the correct balance between the input signal level at the detector and the set-point voltage.
The basic connections for operating the ADL5330 in an AGC loop with the AD8318 are shown in Figure 1. The AD8318 is a 1 MHz to 8 GHz precision demodulating logarithmic amplifier. It offers a large detection range of 60 dB with ±0.5 dB temperature stability. The gain control pin of the ADL5330 is controlled by the output pin of the AD8318. This voltage, VOUT, has a range of 0 V to near VPOS. To avoid overdrive recovery issues, the AD8318 output voltage can be scaled down using a resistive divider to interface with the 0 V to 1.4 V gain control range of ADL5330.
A coupler/attenuation of 23 dB is used to match the desired maximum output power from the VGA to the top end of the linear operating range of the AD8318 (at approximately −5 dBm at 900 MHz).
The detector’s error amplifier uses CFLT, a ground-referenced capacitor pin, to integrate the error signal (in the form of a current). A capacitor must be connected to CFLT to set the loop bandwidth and to ensure loop stability.
Figure 2 shows the transfer function of the output power vs. the VSET voltage over temperature for a 900 MHz sine wave with an input power of −1.5 dBm. Note that the power control of the AD8318 has a negative sense. Decreasing VSET, which corresponds to demanding a higher signal from the ADL5330, tends to increase GAIN.
Stable, Closed-Loop Automatic Power Control for RF (CN0050)
Figure 2: ADL5330 Output Power vs. AD8318 Setpoint Voltage, PIN = -1.5 dBm
The AGC loop is capable of controlling signals just under the full 60 dB gain control range of the ADL5330. The performance over temperature is most accurate over the highest power range, where it is generally most critical. Across the top 40 dB range of output power, the linear conformance error is well within ±0.5 dB over temperature.
The broadband noise added by the logarithmic amplifier is negligible.
In order for the AGC loop to remain in equilibrium, the AD8318 must track the envelope of the ADL5330 output signal and provide the necessary voltage levels to the ADL5330’s gain control input. Figure 3 shows an oscilloscope screenshot of the AGC loop depicted in Figure 1. A 100 MHz sine wave with 50% AM modulation is applied to the ADL5330. The output signal from the ADL5330 is a constant envelope sine wave with amplitude corresponding to a setpoint voltage at the AD8318 of 1.5 V. Also shown is the gain control response of the AD8318 to the changing input envelope.
Stable, Closed-Loop Automatic Power Control for RF (CN0050)
Figure 3: Oscilloscope Screenshot Showing an AM Modulated Input Signal
Figure 4 shows the response of the AGC RF output to a pulse on VSET. As VSET decreases to 1 V, the AGC loop responds with an RF burst. Response time and the amount of signal integration are controlled by the capacitance at the AD8318 CFLT pin—a function analogous to the feedback capacitor around an integrating amplifier. An increase in the capacitance results in slower response time.
This circuit can be used to implement a constant power out function (fixed setpoint with variable input power) or a variable power out function (variable setpoint with fixed or variable input power). If a lower output power control range is desired, the AD8318 log amp (60 dB power detection range) can be replaced with either the AD8317 (50 dB power detection range) or the AD8319 (45 dB power detection range). For a constant output power function, the lowest dynamic range detector (AD8319) will be adequate since the loop will always servo the detector’s input power to a constant level.
The ADL5330 VGA which is optimized for transmit applications can be replaced by the AD8368 VGA. The AD8368 is optimized for receive applications low frequencies up to 800 MHz and provides 34 dB of linear-in-dB voltage-controlled variable gain.
Contributed October, 2008
On This Page:
Ask the Experts/Provide Feedback
Have questions
about this circuit or your upcoming design? Please contact
our experienced applications engineers who are readily available to assist you.
Have feedback on this circuit? Please provide it
here.
-
AD8317:
1 MHz to 10 GHz, 50 dB Log Detector/ControllerThe AD8317 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs the progressive compression technique over a cascaded amplifier chain, each stage of which is equipped with a detector cell. The device can be used in either measurement or controller modes. The AD8317 maintains accurate log conformance for More
Data Sheet Rev B, 03/2008 (pdf 775kB)
Data Sheet Rev B, 03/2008 (pdf 775kB) -
AD8318:
1 MHz to 8 GHz, 70 dB Logarithmic Detector/ControllerThe AD8318 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output voltage. It employs the progressive compression technique over a cascaded amplifier chain, each stage of which is equipped with a detector cell. The device is used in measurement or controller mode. The AD8318 maintains accurate log conformance for More
Data Sheet Rev B, 04/2007 (pdf 2000kB)
Data Sheet Rev B, 04/2007 (pdf 2000kB) -
AD8319:
1 MHz to 10 GHz, 40 dB Log Detector/ControllerThe AD8319 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs the progressive compression technique over a cascaded amplifier chain, each stage of which is equipped with a detector cell. The device can be used in either measurement or controller modes. The AD8319 maintains accurate log conformance for More
Data Sheet Rev B, 04/2008 (pdf 1310kB)
Data Sheet Rev B, 04/2008 (pdf 1310kB) -
ADL5330:
10 MHz to 3 GHz VGA with 60dB Gain Control RangeThe ADL5330 is a broadband voltage variable gain amplifier specified for operation from 10MHz to 3GHz. The device provides precise linear-in-dB gain control over 60dB range with approximately -40dB attenuation and +20dB gain. A 0 to 1.4V gain control input voltage is required to set the gain or attenuation over the 60db range.
The ADL5330 provides a high linearity output power making the More
Data Sheet Rev A, 06/2005 (pdf 863kB)
Data Sheet Rev A, 06/2005 (pdf 863kB)
Evaluation Boards
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- ADIsimPLL™ ADIsimPLL enables the rapid and reliable evaluation of new high performance...
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
ADIsimRF
ADI’s ADIsimRF design tool provides calculations for the most important par...