-
Products
- Amplifiers and Comparators
- Analog Microcontrollers
- Analog to Digital Converters
- Audio/Video Products
- Broadband Products
- Clock and Timing
- Digital to Analog Converters
- Embedded Processing and DSP
- Fiber/Optic
- Interface
- MEMS
- Power Management
- References
- RF/IF Components
- Sensors
- Switches/Multiplexers
- Temperature Sensing and Thermal Management
- Other Products
- Analog/HDMI/DVI Interfaces
- Audio A/D Converters
- Audio Amplifiers
- Audio CODECs
- Audio D/A Converters
- Audio Signal Processors
- Camera/Camcorder Analog Front Ends
- Display Driver Electronics
- iMEMS® Microphone
- Lens Driver Components
- Mobile TV Tuners
- Sample Rate Converters
- Video Amps/Buffers/Filters
- Video CODECs
- Video Compression
- Video Decoders
- Video Encoders
OTHERS WAYS
TO FIND PRODUCTSSelection Guides Product Selection Tables - Resources & Tools
-
About ADI
- My Analog
ADI engineers share their lab work with you in this
‘Circuits from the Lab’ Circuit Note.
You can combine these product pairings quickly and with confidence.
Please review our Circuits from the Lab Information and Disclaimer page
for more details.
CN0046
ADI engineers share their lab work with you in this ‘Circuits from the Lab’ Circuit Note. You can combine these product pairings quickly and with confidence. Please review the disclaimer at the bottom of the page for more information.
Copyright 2008, Analog Devices, Inc. All rights reserved. "Circuits from the Lab" from Analog Devices have been designed and built by Analog Devices engineers. Standard engineering practices have been employed in the design and construction of each circuit, and their function and performance have been tested and verified in a lab environment at room temperature. However, you are solely responsible for testing the circuit and determining its suitability and applicability for your use and application. Accordingly, in no event shall Analog Devices be liable for direct, indirect, special, incidental, consequential or punitive damages due to any cause whatsoever connected to the use of any "Circuits from the Lab". Circuit variations described in the Common Variations section of the document have not necessarily also been built and tested.
"Circuits from the Lab" are intended only for use with Analog Devices products and are the intellectual property of Analog Devices or its licensors. While you may use the "Circuits from the Lab" in the design of your product, no other license is granted by implication or otherwise under any patents or other intellectual property by application or use of the "Circuits from the Lab". Information furnished by Analog Devices is believed to be accurate and reliable. However, "Circuits from the Lab" are supplied "as is" and without warranties of any kind, express, implied, or statutory including, but not limited to, any implied warranty of merchantability, noninfringement or fitness for a particular purpose and no responsibility is assumed by Analog Devices for their use, nor for any infringements of patents or other rights of third parties that may result from their use. Analog Devices reserves the right to change any "Circuits from the Lab" at any time without notice, but is under no obligation to do so. Trademarks and registered trademarks are the property of their respective owners.
Using the AD8352 as an Ultralow Distortion Differential RF/IF Front End for High Speed ADCs
  (CN0046)| Circuit Types: | ADC Circuit/Driver |
| Optimized For: | High Speed, Low Noise and Distortion |
| Applications: | Communications, Medical, Optical |
These circuits provide both a single-ended and a differential configuration for driving high speed ADCs using the AD8352 ultralow distortion differential RF/IF amplifier. The AD8352 provides the gain, isolation, and distortion performance necessary for efficiently driving high linearity converters, such as the AD9445. This device also provides balanced outputs whether driven differentially or single-ended, thereby maintaining excellent second-order distortion levels.
Using the AD8352 as an Ultralow Distortion Differential RF/IF Front End for High Speed ADCs (CN0046)
Figure 1. Differential Input to the AD8352 Driving the AD9445 14-Bit, 105 MSPS/125 MSPS ADC (Simplified Schematic, All Connections Not Shown)
Figure 1 and Figure 2 illustrate two front-end circuits for driving the AD9445 14-bit ADC at 105 MSPS. Figure 1 provides a differential input configuration, while Figure 2 provides a single-ended input configuration.
Using the AD8352 as an Ultralow Distortion Differential RF/IF Front End for High Speed ADCs (CN0046)
Figure 2. Single-Ended Input to the AD8352 Driving the AD9445 ADC (Simplified Schematic, All Connections Not Shown)
In the differential configuration shown in Figure 1, the input 49.9 Ω resistor provides a differential input impedance to the 50 Ω RF/IF source. When the driver is located less than approximately one eighth of the wavelength of the maximum input RF/IF frequency from the AD8352, impedance matching is not required, thereby eliminating the need for this termination resistor. The output 24 Ω series resistors provide isolation from the input capacitance of the ADC, and the optimum value is determined empirically. The 100 MHz FFT plots shown in Figure 3 and Figure 4 display the performance results for the differential configuration.
In the single-ended input configuration shown in Figure 2, the net input impedance at VIP is RN (200 Ω) plus the external 24.9 Ω balancing resistor, or ~225 Ω. This requires a 64.9 Ω parallel resistor to provide the input impedance match for a 50 Ω source. If input reflections are minimal, this impedance match is not required. The 200 Ω resistor (RN) is required to balance the output voltages to minimize second-order distortion.
The single-ended configuration provides −3 dB bandwidths similar to input differential drive and shows little or no degradation in overall third-order harmonic performance. The single-ended, third-order distortion levels are similar to the differential FFT plots in Figure 3 and Figure 4. The single-ended circuit avoids the use of a transformer or balun in front of the amplifier while still maintaining excellent distortion up to approximately 100 MHz. However, at frequencies above approximately 100 MHz, second-order distortion increases when the AD8352 is driven single-ended due to phase-related errors.
Using the AD8352 as an Ultralow Distortion Differential RF/IF Front End for High Speed ADCs (CN0046)
Figure 3. Single Tone Distortion, AD8352 Driving AD9445, Sampling Clock = 105 MSPS, Analog Input Frequency = 100 MHz, AV = 10 dB. See Figure 1.
In both configurations, RG is the gain setting resistor for the AD8352, with the RD and CD components providing distortion cancellation. The AD9445 differential input impedance is approximately 2 kΩ in parallel with 5 pF and requires a 2.0 V p-p differential signal (VREF = 1 V) between VIN+ and VIN− for a full-scale input signal.
The output of the amplifier is ac-coupled to allow for an optimum common-mode voltage at the ADC input. The common-mode voltage at the input of the AD9445 is set to 3.5 V by an internal network. Input ac-coupling can be required if the source also requires a common-mode voltage that is outside the optimum range of the AD8352. A VCM common-mode pin is provided on the AD8352 that equally shifts both input and output common-mode levels. Increasing the gain of the AD8352 increases the system noise and, thus, decreases the SNR (3.5 dB at 100 MHz input for AV = 10 dB) of the AD9445 when no filtering is used. However, it should be noted that amplifier gains from 3 dB to 18 dB, with proper selection of CD and RD, do not appreciably affect distortion levels. These circuits, when configured properly, can result in SFDR performance of better than 87 dBc at 70 MHz and 82 dBc at 180 MHz input. Single-ended drive, with appropriate CD and RD, gives similar results for SFDR and third-order intermodulation levels as shown in these figures.
Excellent layout, grounding, and decoupling techniques must be utilized in order to achieve the desired performance from the circuits discussed in this note. As a minimum, a 4-layer PCB should be used with one ground plane layer, one power plane layer, and two signal layers.
All IC power pins must be decoupled to the ground plane with low inductance multilayer ceramic capacitors (MLCC) of 0.01 μF to 0.1 μF (this is not shown in the diagrams for simplicity). Follow the recommendations on the individual data sheets for the ICs.
The product evaluation boards should be consulted for recommended layout and critical component placement. They can be accessed through the main product pages for the devices or their data sheets.
Using the AD8352 as an Ultralow Distortion Differential RF/IF Front End for High Speed ADCs (CN0046)
Figure 4. Two Tone Intermodulation Distortion, AD8352 Driving AD9445, Sampling Clock = 105 MSPS, Analog Input Frequency = 98 MHz and 101 MHz, AV = 10 dB. See Figure 1.
Placing antialiasing filters between the ADC and the amplifier is a common approach for improving overall noise and broadband distortion performance for both band-pass and low-pass applications. For high frequency filtering, matching to the filter is required. The AD8352 maintains a 100 Ω output impedance well beyond most applications and is well-suited to drive most filter configurations with little or no degradation in distortion.
The AD8352 low distortion differential amplifier can be replaced by the high IP3, low noise figure AD8375 variable gain amplifier (VGA). The AD8375 is a digitally controlled, variable gain, wide bandwidth amplifier that provides precise gain control across a broad 24 dB gain range, with 1 dB resolution. The AD8376 is a dual version of the AD8375. (See Circuit Note CN-0002, Using the AD8376 VGA to Drive Wide Bandwidth ADCs for High IF AC-Coupled Applications.).
Contributed October, 2008
On This Page:
Ask the Experts/Provide Feedback
Have questions
about this circuit or your upcoming design? Please contact
our experienced applications engineers who are readily available to assist you.
Have feedback on this circuit? Please provide it
here.
-
AD8352:
2 GHz Ultralow Distortion Differential RF/IF AmplifierThe AD8352 is a high performance differential amplifier optimized for RF and IF applications. It achieves better than 80 dB SFDR performance at frequencies up to 200 MHz, and 65 dB beyond 500 MHz, making it an ideal driver for high speed 12-bit to 16-bit analog-to-digital converters (ADCs).
Unlike other wideband differential amplifiers, the AD8352 has buffers that isolate the gain setting More
Data Sheet Rev B, 07/2008 (pdf 1233kB)
Data Sheet Rev B, 07/2008 (pdf 1233kB) -
AD9445:
14-Bit, 105 MSPS / 125 MSPS A/D ConverterThe AD9445 is a 14-bit monolithic, sampling analog-to-digital converter (ADC) with an on-chip, IF sampling track-and-hold circuit and is optimized for power, small size, and ease of use. The product operates at up to an 105 MSPS conversion rate and is optimized for multi-carrier, multimode receivers, such as those found in cellular infrastructure equipment.
The ADC requires 3.3 V and 5.0 V More
Data Sheet Rev 0, 11/2005 (pdf 965kB)
Data Sheet Rev 0, 11/2005 (pdf 965kB)
Evaluation Boards
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- High Speed ADC Evaluation Board Software and Behavioral Models
- ADIsimPLL™ ADIsimPLL enables the rapid and reliable evaluation of new high performance...
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
ADIsimRF
ADI’s ADIsimRF design tool provides calculations for the most important par...
- High Speed ADC Evaluation Board Software and Behavioral Models
- AD9445 IBIS Models