-
Products
- Amplifiers and Comparators
- Analog Microcontrollers
- Analog to Digital Converters
- Audio/Video Products
- Broadband Products
- Clock and Timing
- Digital to Analog Converters
- Embedded Processing and DSP
- Fiber/Optic
- Interface
- MEMS
- Power Management
- References
- RF/IF Components
- Sensors
- Switches/Multiplexers
- Temperature Sensing and Thermal Management
- Other Products
- Analog/HDMI/DVI Interfaces
- Audio A/D Converters
- Audio Amplifiers
- Audio CODECs
- Audio D/A Converters
- Audio Signal Processors
- Camera/Camcorder Analog Front Ends
- Display Driver Electronics
- iMEMS® Microphone
- Lens Driver Components
- Mobile TV Tuners
- Sample Rate Converters
- Video Amps/Buffers/Filters
- Video CODECs
- Video Compression
- Video Decoders
- Video Encoders
OTHERS WAYS
TO FIND PRODUCTSSelection Guides Product Selection Tables - Resources & Tools
-
About ADI
- My Analog
ADI engineers share their lab work with you in this
‘Circuits from the Lab’ Circuit Note.
You can combine these product pairings quickly and with confidence.
Please review our Circuits from the Lab Information and Disclaimer page
for more details.
CN0044
ADI engineers share their lab work with you in this ‘Circuits from the Lab’ Circuit Note. You can combine these product pairings quickly and with confidence. Please review the disclaimer at the bottom of the page for more information.
Copyright 2008, Analog Devices, Inc. All rights reserved. "Circuits from the Lab" from Analog Devices have been designed and built by Analog Devices engineers. Standard engineering practices have been employed in the design and construction of each circuit, and their function and performance have been tested and verified in a lab environment at room temperature. However, you are solely responsible for testing the circuit and determining its suitability and applicability for your use and application. Accordingly, in no event shall Analog Devices be liable for direct, indirect, special, incidental, consequential or punitive damages due to any cause whatsoever connected to the use of any "Circuits from the Lab". Circuit variations described in the Common Variations section of the document have not necessarily also been built and tested.
"Circuits from the Lab" are intended only for use with Analog Devices products and are the intellectual property of Analog Devices or its licensors. While you may use the "Circuits from the Lab" in the design of your product, no other license is granted by implication or otherwise under any patents or other intellectual property by application or use of the "Circuits from the Lab". Information furnished by Analog Devices is believed to be accurate and reliable. However, "Circuits from the Lab" are supplied "as is" and without warranties of any kind, express, implied, or statutory including, but not limited to, any implied warranty of merchantability, noninfringement or fitness for a particular purpose and no responsibility is assumed by Analog Devices for their use, nor for any infringements of patents or other rights of third parties that may result from their use. Analog Devices reserves the right to change any "Circuits from the Lab" at any time without notice, but is under no obligation to do so. Trademarks and registered trademarks are the property of their respective owners.
Using the AD8599 Op Amp as an Ultralow Distortion Driver for the AD7995
  (CN0044)| Circuit Types: | ADC Circuit/Driver |
| Optimized For: | High Speed, Low Noise and Distortion |
| Applications: | Building Controls, Communications, Instrumentation, Medical, Motion Control, Process Control |
The circuit described in this document provides an ultralow distortion driver circuit for the AD7995 10-bit, 4-channel ADC, which is designed to achieve optimum ac and dc performance. The circuit uses the ultralow distortion, ultralow noise AD8599 dual-supply op amp and ultrahigh precision AD780 band gap voltage reference to ensure that the maximum AD7995 performance is achieved, by providing a low impedance driver with adequate settling time and a highly accurate reference voltage. The AD8599 is a dual operational amplifier that operates with supplies from ±4.5 V to ±18 V. The AD7995 has an I2C-compatible serial interface and is offered in an 8-lead SOT-23 package.
Using the AD8599 Op Amp as an Ultralow Distortion Driver for the AD7995  (CN0044)
Figure 1: AD7995 ADC with the AD8599 Low Distortion Driver and AD780 Ultrahigh Precision Reference (Simplified Schematic: Decoupling and All Connections Not Shown)
It is always recommended to buffer analog input signals before applying them to ADCs with switched capacitor inputs such as the AD7995. This is particularly important in applications where the signal source has high source impedance and where low distortion and high signal-to-noise-ratio is important. The circuit illustrated in Figure 1 shows how the AD8599, an ideal choice for high accuracy designs, can be used to buffer the analog input channels.
The AD7995 can be operated as a 4-channel input device using VDD as a reference (the input voltage range is 0 V to VDD) or as a 3-channel input device with the fourth channel used as an external reference input, VREF (the input range is 0 V to VREF). These options are programmable via the I2C-compatible interface.
The AD780 is a 2.5 V/3 V ultrahigh precision, band gap voltage reference and is recommended for use with AD7995. A 1 μF decoupling capacitor is recommended on the VIN3 / VREF signal for best performance.
Care must be taken to ensure that the analog input signal to the ADC does not exceed the supply rails by more than 300 mV. If the signal does exceed this level, the internal ESD protection diodes become forward-biased and start conducting current into the substrate. Each diode can conduct a maximum current of 10 mA without causing irreversible damage to the part. The MT-036 Tutorial discusses methods to protect the input circuits of op amps and ADCs against such damage.
In addition, the circuit must be constructed on a multilayer PC board with a large area ground plane. Proper layout, grounding, and decoupling techniques must be used to achieve optimum performance (see MT-031 Tutorial, MT-101 Tutorial, and the AD7995 evaluation board layout).
If single-supply op amp operation is required for buffering the input signal, the AD8605 is a suitable choice. Note that the output of the AD8605 operating on a single +5 V supply can only go to approximately 20 mV above ground; therefore, the AD7995 input range from 0 V to +20 mV cannot be exercised (see MT-035 Tutorial).
The AD7995 can accept a reference input voltage from 1.2 V to VDD; therefore, different voltage reference sources can be used.
Contributed October, 2008
On This Page:
Ask the Experts/Provide Feedback
Have questions
about this circuit or your upcoming design? Please contact
our experienced applications engineers who are readily available to assist you.
Have feedback on this circuit? Please provide it
here.
-
AD780:
2.5 V/3.0 V Ultrahigh Precision Bandgap Voltage ReferenceThe AD780 is an ultrahigh precision bandgap reference voltage which provides a 2.5 V or 3.0 V output from inputs between 4.0 V and 36 V. Low initial error and temperature drift combined with low output noise and the ability to drive any value of capacitance make the AD780 the ideal choice for enhancing the performance of high resolution ADCs and DACs and for any general purpose precision reference More
Data Sheet Rev E, 05/2004 (pdf 375kB)
Data Sheet Rev E, 05/2004 (pdf 375kB) -
AD7995:
4-Channel, 10-Bit ADC with I2C Compatible Interface in 8-Lead SOT-23The AD7991/AD7995/AD7999 are 12-/10-/8-bit, low power, successive approximation ADCs with an I2C®-compatible interface. Each part operates from a single 2.7 V to 5.5 V power supply and features a 1 μs conversion time. The track-and-hold amplifier allows each part to handle input frequencies of up to 14 MHz, and a multiplexer allows taking samples from four channels.
Each More
Data Sheet Rev A, 10/2009 (pdf 776kB)
Data Sheet Rev A, 10/2009 (pdf 776kB) -
AD8599:
Dual, Ultralow Distortion, Ultralow Noise Op AmpThe AD8597/AD8599 are very low noise, low distortion opera-tional amplifiers ideal for use as preamplifiers. The low noise of 1.1 nV/√Hz and low harmonic distortion of −120 dB (or better) at audio bandwidths give the AD8597/AD8599 the wide dynamic range necessary for preamplifiers in audio, medical, and instru-mentation applications. The excellent slew rate of 14 V/μs and 10 MHz gain bandwidth More
Data Sheet Rev B, 11/2008 (pdf 534kB)
Data Sheet Rev B, 11/2008 (pdf 534kB)
Evaluation Boards
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- EVAL-AD7991/AD7995: Evaluation Board for the 4-Channel,
12-Bit/10-Bit ADC with I2C-Compatible Interface
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- Voltage Reference Wizard This Wizard helps you select the most suitable voltage for a use with a dat...
- AD780 SPICE Macro-Model
- AD8599 SPICE Macro Model
- AD8599 SPICE Macro Model