-
Products
- Amplifiers and Comparators
- Analog Microcontrollers
- Analog to Digital Converters
- Audio/Video Products
- Broadband Products
- Clock and Timing
- Digital to Analog Converters
- Embedded Processing and DSP
- Fiber/Optic
- Interface
- MEMS
- Power Management
- References
- RF/IF Components
- Sensors
- Switches/Multiplexers
- Temperature Sensing and Thermal Management
- Other Products
- Analog/HDMI/DVI Interfaces
- Audio A/D Converters
- Audio Amplifiers
- Audio CODECs
- Audio D/A Converters
- Audio Signal Processors
- Camera/Camcorder Analog Front Ends
- Display Driver Electronics
- iMEMS® Microphone
- Lens Driver Components
- Mobile TV Tuners
- Sample Rate Converters
- Video Amps/Buffers/Filters
- Video CODECs
- Video Compression
- Video Decoders
- Video Encoders
OTHERS WAYS
TO FIND PRODUCTSSelection Guides Product Selection Tables - Resources & Tools
-
About ADI
- My Analog
ADI engineers share their lab work with you in this
‘Circuits from the Lab’ Circuit Note.
You can combine these product pairings quickly and with confidence.
Please review our Circuits from the Lab Information and Disclaimer page
for more details.
CN0009
ADI engineers share their lab work with you in this ‘Circuits from the Lab’ Circuit Note. You can combine these product pairings quickly and with confidence. Please review the disclaimer at the bottom of the page for more information.
Copyright 2008, Analog Devices, Inc. All rights reserved. "Circuits from the Lab" from Analog Devices have been designed and built by Analog Devices engineers. Standard engineering practices have been employed in the design and construction of each circuit, and their function and performance have been tested and verified in a lab environment at room temperature. However, you are solely responsible for testing the circuit and determining its suitability and applicability for your use and application. Accordingly, in no event shall Analog Devices be liable for direct, indirect, special, incidental, consequential or punitive damages due to any cause whatsoever connected to the use of any "Circuits from the Lab". Circuit variations described in the Common Variations section of the document have not necessarily also been built and tested.
"Circuits from the Lab" are intended only for use with Analog Devices products and are the intellectual property of Analog Devices or its licensors. While you may use the "Circuits from the Lab" in the design of your product, no other license is granted by implication or otherwise under any patents or other intellectual property by application or use of the "Circuits from the Lab". Information furnished by Analog Devices is believed to be accurate and reliable. However, "Circuits from the Lab" are supplied "as is" and without warranties of any kind, express, implied, or statutory including, but not limited to, any implied warranty of merchantability, noninfringement or fitness for a particular purpose and no responsibility is assumed by Analog Devices for their use, nor for any infringements of patents or other rights of third parties that may result from their use. Analog Devices reserves the right to change any "Circuits from the Lab" at any time without notice, but is under no obligation to do so. Trademarks and registered trademarks are the property of their respective owners.
| Circuit Types: | Multiplying |
| Optimized For: | Isolation |
| Applications: | Process Control |
In many process control applications, 2-wire current transmitters are often used to transmit analog signals through noisy environments. These current transmitters use a zero-scale signal current of 4 mA and a full-scale signal current of 20 mAhence the designation "4 mA to 20 mA converter." The circuit described in this document provides a low power current transmitter with 16-bit resolution and monotonicity, which is powered directly from the 4 mA to 20 mA control loop power supply and consumes less than 4 mA. Transmitters requiring more than 4 mA cannot be powered directly from the loop power supply and, therefore, require an additional supply.
This circuit provides a programmable output current of 4 mA to 20 mA using the AD5662 nanoDAC converter as a controller. The loop current is sensed by measuring the voltage, VOUT, which is dropped across RS. If the DAC output is 0 V, a current of
![]()
flows through R2 and R3, forcing the PCB ground to be 349 mV more positive than the voltage measured at the load side of RS. This corresponds to a loop current of
![]()
When the DAC outputs a full-scale voltage of 5 V, the current through R2 is
![]()
The current through R1 is
![]()
Therefore, the current through R3 is
![]()
This forces the voltage, VOUT, across RS to equal
![]()
The feedback loop around the AD8627 forces the voltage at its noninverting input to equal the PCB ground voltage. The output current is, therefore, directly proportional to the digital code. The AD8627 regulates the DAC output current to satisfy the current summation at its noninverting node. The output current is calculated using the following equation:
![]()
For the values shown in Figure 1
![]()
where 0 ≤ D ≤ 65,535. This circuit gives a full-scale output current of 20.9 mA when the AD5662 digital code equals 0xFFFF. Likewise, the output current will be 3.49 mA when the AD5662’s digital code equals 0x0000. The extended current range (3.49 mA to 20.9 mA) allows the user to calibrate the 4 mA to 20 mA range by using software and the 16-bit resolution of the AD5662. The Schottky diode is required in this circuit to prevent loop supply power-on transients from pulling the noninverting input of the AD8627 more than 300 mV below its inverting input. The Schottky diode must be able to handle at least the 20 mA full loop load.
Biasing for the controller is provided by the ADR02 precision 5 V reference, and the circuit requires no external trims because of the tight initial output voltage tolerance of the ADR02 and the low supply current of both the AD8627 and the AD5662.
The limits on the allowable loop power supply are set by the ADR02 minimum input voltage (7 V) and maximum input voltage (36 V). The 2N3904 maximum allowable power dissipation at 25°C is 625 mW, so a higher power transistor must be used if the loop supply exceeds about 30 V. Power dissipation in the 2N3904 can be reduced by adding an appropriate voltage dropping resistor in series with its collector.
The basic circuit is flexible and can accommodate a number of different references, voltage output DACs, and op amps. Considerations are reference accuracy, DAC resolution, and amplifier offset voltage. The prime requirement is that the total circuit must operate on the loop supply voltage and require less than 4 mA quiescent current (for a DAC code of 0x0000).
Contributed May, 2009
On This Page:
Ask the Experts/Provide Feedback
Have questions
about this circuit or your upcoming design? Please contact
our experienced applications engineers who are readily available to assist you.
Have feedback on this circuit? Please provide it
here.
-
AD5662:
2.7-5.5V, 16-Bit nanoDAC® Converter in a Sot-23The AD5662, a member of the nanoDAC® family of devices, is a low cost, low power, single 16-bit buffered voltage-out guaranteed monotonic DAC.
The part incorporates a power-on-reset circuit that depending on model ensures that the DAC output powers up to zero volts or midscale and remains there until a valid write takes place. Power consumption is typically 250 µA and the part More
Data Sheet Rev 0, 02/2005 (pdf 834kB)
Data Sheet Rev 0, 02/2005 (pdf 834kB) -
AD8627:
Precision, Low Power, Single Supply JFET Amplifier in 5-Lead SC70The AD8627 is a true single supply precision JFET input amplifier featuring low power consumption and rail-to-rail output. Outputs are stable with capacitive loads of over 500 pF. Supply current is less than 900 µA per amplifier.
Applications for these amplifiers include photodiode transimpedance amplification, ATE reference level drivers, battery management, both line powered and More
Data Sheet Rev D, 03/2009 (pdf 442kB)
Data Sheet Rev D, 03/2009 (pdf 442kB) -
ADR02:
Ultracompact, Precision 5.0 V Voltage ReferenceThe ADR01, ADR02, ADR03, and ADR06 are precision 10.0 V, 5.0 V, 2.5 V, and 3.0 V band gap voltage references featuring high accuracy, high stability, and low power consumption. The parts are housed in tiny, 5-lead SC70 and TSOT packages, as well as in 8-lead SOIC versions. The SOIC versions of the ADR01, ADR02, and ADR03 are drop-in replacements1 to the industry-standard REF01, REF02, More
Data Sheet Rev L, 12/2008 (pdf 738kB)
Data Sheet Rev L, 12/2008 (pdf 738kB) -
ADUM1300:
Triple-Channel Digital IsolatorThe ADuM130x* are triple-channel digital isolators based on the Analog Devices, Inc., iCoupler® technology. Combining high speed CMOS and monolithic transformer technology, these isolation components provide outstanding performance characteristics superior to alternatives, such as optocouplers.
By avoiding the use of LEDs and photodiodes, More
Data Sheet Rev H, 05/2008 (pdf 708kB)
Data Sheet Rev H, 05/2008 (pdf 708kB)
Evaluation Boards
- AD5620/AD5640/AD5660/AD5662 Evaluation Tools
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- ADuM5401-ADuM5404 Evaluation Tools Evaluation Board for the ADuM5401-ADuM5404 Quad Isolators with isoPo...
- PLC DEMO SYSTEM
- ADIsimPower™ Voltage Regulator Design Tool This tool supports buck converter designs OPTIMIZED for efficiency, PCB spa...
- iCoupler™ Current Consumption Calculator An online tool to calculate current consumption in ADI's digital isolators.
- Voltage Reference Wizard This Wizard helps you select the most suitable voltage for a use with a dat...
- AD8627 SPICE Macro Model
- ADuM1300 IBIS Model (All Speed Grades)
- Analog Bridge Wizard The Analog Bridge Wizard recommends amplifiers and ADC's for your bridge ap...