Glossary of EE Terms

Term

If you would like to suggest new
glossary terms, please contact us.

  • Effective Number of Bits (ENOB)

    When operating with real-world signals, non-ideal behavior in the ADC or DAC degrades the device performance. This degradation can be modeled as a loss of resolution, and the ENOB specification describes the achievable performance that is realizable, regardless of the actual number of bits within the ADC or DAC. The ENOB can be calculated from the signal-to-noise and distortion ratio (SINAD) based on the equation:

    ENOB
  • EIN

    EIN stands for Equivalent Input Noise, the noise created by the microphone expressed as an external noise source placed at the microphone's input.

  • Encode Pulse Width (Duty Cycle)

    Pulse width high is the minimum amount of time that the ENCODE pulse should be left in logic "1" state to achieve rated performance; pulse width low is the minimum time ENCODE pulse should be left in low state. At a give clock rate, these specs define an acceptable Encode duty cycle.

  • ESD

    Electrostatic discharge is the transfer of an electrostatic charge between two objects. This is a very rapid event that happens when two objects of different potentials come into direct contact with each other. ESD is one of the most common causes of electronic equipment damage or malfunction. Walking or working on a grounded ESD mat drains the electrical charge before it damages any ESD sensitive devices. There are three types of static control mats that are classified by their surface resistivity range. Surface resistivity is express in ohms (Ω). It measures how much a surface resists draining a static charge. The lower the surface resistivity the faster and more effective the mats will dissipate the Electrostatic charge.


Send Feedback X
content here.
content here.

Send Feedback

Close