FAQs/RAQs (9)
- Could software be used to eliminate competitor mics’ response peaks?
- Is a microphone with -37 dBV sensitivity better than a microphone with -42 dBV (lower) sensitivity?
- Why not design a mic with the highest sensitivity?
- Due to open package, are there problems with humidity (condensation) when cooling down/heating up the device?
- Can ADI MEMS mics be soldered to a flex PCB?
- What is the recommended thickness of the PCB for the ADI MEMS mics?
- Could direct soldering to a PCB cause vibration pickup by the mic?
- Can digital microphone PDM output be interfaced with I²S directly?
- Is -26 dBFS digital mic sensitivity higher than -42 dBV analog mic sensitivity?