Technical Articles (25)
- MS-2393: MEMS Enable Medical Innovation (pdf, 232 kB)
-
Blackbox Biometrics testing ADI MEMS for Blast Gauge Monitor
EE Times, June 2012 -
Soldier-worn sensor that measures the destructive power of explosives uses MEMS accelerometer from Analog Devices
Military & Aerospace Electronics, June 2012 -
Microelectronic Sensing System Enables In-Flight Arrow Ballistics Measurement
(EE Times, 4/29/2012) - MS-2115: The Pursuit of Accurate and Reliable Vibration Sensing For Condition-Based Predictive Maintenance (pdf, 291 kB)
- Inertial Sensors Go Hollywood (pdf, 349 kB)
-
Pursuing Accurate, Reliable Vibration Sensing for Condition-Based Predictive Maintenance
Sensors, January 2011 - Inertial MEMS, from Life-Enhancing to Life-Saving, MS-2202 (pdf, 60 kB)
- MS-2163: Improving Industrial Control with Integrated MEMS Inertial Sensors (pdf, 104 kB)
- Basic Linear Design: Chapter 3 Sensors Section 3.1: Positional Sensors
-
Power Cycling 101: Optimizing Energy Use in Advanced Sensor Products
(Analog Dialogue, August 2010) -
Full-Featured Pedometer Design Realized with 3-Axis Digital Accelerometer
(pdf, 598 kB)
Analog Dialogue, June 2010 -
The Five Motion Senses: MEMS Inertial Sensing to Transform Applications
The introduction of robust, low-cost MEMS accelerometers and gyroscopes enables the incorporation of motion sensing into a greater variety of applications.
(Sensors, 1/1/2010 -
Cannondale’s New Simon Device Takes Bike Suspension to the Next Level
(Venturebeat, January 2010) -
Analog Devices Accelerometer Adds Intelligent Sensing to Mountain Bike Suspension System
(MEMS Industry Group, January 2010) -
Precision Tilt/Fall Detector Consumes Less Than 1.5 mW
When you need to detect angular position related to Earth’s gravity, you can use an Analog Devices three-axis MEMS (microelectromechanical-system) accelerometer.
(EDN, 12/3/2009) -
Human Fall Detection Using New MEMS Accelerometer Technology
For humans, an unobserved fall can have very serious consequences. Statistics show that the majority of serious consequences are not the direct result of falling, but rather are due to a delay in assistance and treatment. Post-fall consequences can be greatly reduced if relief personnel can be alerted in time.
(ECN, December 9, 2009) - "Technology Vendors Go to Hollywood", Coverage of ADI’s MEMS used in filming of Harry Potter
-
MEMS Accelerometer Calibration Optimizes Accuracy for Industrial Applications
(Industrial Control Designline, 10/07) -
Accelerometers--Fantasy & Reality
(Analog Dialogue, May 2009) -
Sonic Nirvana: MEMS Accelerometers as Acoustic Pickups in Musical Instruments
MEMS sensors are in our cars, phones, PCs, cameras, and a variety of other applications but until now, they've never been attached to a guitar. The authors seek to answer the question: Can you use a MEMS accelerometer as an acoustic transducer?
(Sensors, June 2009) - Patient Respiration Measurement Using a 3-Axis Accelerometer
-
Making MEMS Accelerometers Work in Motion Control
EETimes Design, 2007 -
iSensor Intelligent Sensor/ADIS16201
Best Product Winner: Electronics -- Design News, March 20, 2006 -
Hot Hands For Some Cool Rock: Motion Sensing Meets Audio Engineering
Electronic Design Magazine, May 2006
Analog Dialogue (4)
- Basic Linear Design: Chapter 3 Sensors Section 3.1: Positional Sensors
-
Full-Featured Pedometer Design Realized with 3-Axis Digital Accelerometer
(pdf, 598 kB)
Analog Dialogue, June 2010 -
Detecting Human Falls with a 3-Axis Digital Accelerometer
(Analog Dialogue, Vol. 43, July 2009) -
Sonic Nirvana: Using MEMS Accelerometers as Acoustic Pickups in Musical Instruments
(Analog Dialogue, Vol. 43, February 2009)
Recommended Reading (4)
- Transitioning from ADXL202 to ADXL213/ADXL203 (pdf, 62 kB)
- It's an Analog World
- Analog Devices Technical Bookstore
-
ADI Warns Against Misuse of COTS Integrated Circuits
(pdf, 13 kB)
(Revised 1/03)
Invites Customer Participation in Creative Mil/Aero System Solutions