LTspice: Simple Steps to Import Third-Party Models

It is possible in LTspice IV to create a new symbol from scratch for a third-party model but who has the time? Follow these easy steps to generate a new symbol for a third-party model defined in a subcircuit (.SUBCKT statement).

  1. Open the netlist file that contains the subcircuit definitions in LTspice (File > Open or drag file into LTspice)
  2. Right-click the line containing the name of the subcircuit, and select Create Symbol:

     

    Create Symbol

    Create Symbol

  3. Edit the symbol if needed and save.

To use the new symbol (and associated third party model) in a schematic, select the symbol from the AutoGenerated directory in the component library (F2) and place it in your schematic:

 

Select Component Symbol
Select Component Symbol

By using the automatic symbol generation you can focus on your simulations, not creating new symbols. For a more information on how to import third party models that use intrinsic SPICE device (.MODEL statement) see the video at www.linear.com/solutions/1083.

Author

Generic_Author_image

Gabino Alonso