Norwood, MA (08/09/2012) - Analog Devices, Inc., ( ADI ), a global leader in high-performance semiconductors for signal-processing applications, today introduced two multiplexers that are able to guarantee latch-up prevention in high-voltage industrial applications operating up to ±22 V. Latch-up, an undesirable high-current state that persists until the power supply is turned off, can lead to device failure.
The ultra-low (0.35 pC) charge injection of the new multiplexers makes them suitable for data acquisition and sample-and-hold applications, where low glitch and fast settling time are required. The low leakage (20 pA) feature ensures high accuracy and resolution, which is an advantage in audio and video signal routing. The ADG5206 and ADG5207 multiplexers are the latest additions to ADI’s switch and multiplexer protection products portfolio, which also includes the ADG5212 and ADG5213—the industry lowest charge injection and low leakage latch-up proof quad switches.
Samples and evaluation board are currently available.
| Part No. | Multiplexer Channels | Availability | Price each in 1,000 quantities | Packaging |
|---|---|---|---|---|
| ADG5206 | 16 | Now | $4.40 | 28-lead TSSOP & LFCSP |
| ADG5207 | Differential 8 | Now | $4.40 | 28-lead TSSOP & LFCSP |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
Doug Bartow
336-605-4145
doug.bartow@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved