ANALOG DEVICES’ MULTIPLEXERS OFFER HIGH ROBUSTNESS, LOW CHARGE INJECTION AND LOW LEAKAGE

ADI’s ADG5206/5207 16-channel and differential 8:1 multiplexers offer guaranteed latch-up protection for industrial, instrumentation and process control applications.

Norwood, MA (08/09/2012) - Analog Devices, Inc., ( ADI ), a global leader in high-performance semiconductors for signal-processing applications, today introduced two multiplexers that are able to guarantee latch-up prevention in high-voltage industrial applications operating up to ±22 V. Latch-up, an undesirable high-current state that persists until the power supply is turned off, can lead to device failure.

  • View the ADG5206 16-channel multiplexer product page, order samples and evaluation boards and download the data sheet
  • View the ADG5207 differential 8:1 multiplexer product page, order samples and evaluation boards and download the data sheet

The ultra-low (0.35 pC) charge injection of the new multiplexers makes them suitable for data acquisition and sample-and-hold applications, where low glitch and fast settling time are required. The low leakage (20 pA) feature ensures high accuracy and resolution, which is an advantage in audio and video signal routing. The ADG5206 and ADG5207 multiplexers are the latest additions to ADI’s switch and multiplexer protection products portfolio, which also includes the ADG5212 and ADG5213—the industry lowest charge injection and low leakage latch-up proof quad switches.

ADG5206 and ADG5207 Features

  • Trench isolation between the N-channel and P-channel transistors of each CMOS switch provides guaranteed latch-up protection
  • Operate from ±9 V to ±22 V in applications where the analog signal is bipolar and from +9 V to +40 V in applications where the analog signal is unipolar
  • Features 3.5-pF off-source capacitance, 60-MHz -3dB bandwidth, ultra-low charge injection (0.35 pC @ 0 V) and source off leakage (400 pA @ 125 °C) performance.
  • Operate equally well in both directions when ON and have an input signal range that extends to the power supplies. In the OFF condition, signal levels up to the supplies are blocked. The switches exhibit break-before-make switching action for use in multiplexer applications.


Pricing and Availability

Samples and evaluation board are currently available.

Part No. Multiplexer Channels Availability Price each in 1,000 quantities Packaging
ADG5206 16 Now $4.40 28-lead TSSOP & LFCSP
ADG5207 Differential 8 Now $4.40 28-lead TSSOP & LFCSP

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Follow ADI on Twitter

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Doug Bartow
336-605-4145

doug.bartow@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close