ANALOG DEVICES ENABLES INDUSTRY’S FASTEST, HIGHEST-RESOLUTION, MULTI-CHANNEL VIDEO DISTRIBUTION SYSTEMS
AD8175/6 triple 16x9 crosspoint switches and AD8145/6/7/8 high-speed differential amplifiers combine to deliver 500-MHz bandwidth supporting UXGA and QXGA resolution in large video displays.
Norwood, MA (02/22/2007) -
Analog Devices today introduced the industry’s first combination of analog crosspoint switches and driver/receiver amplifiers that support bandwidths up to 500 MHz for analog video. Low implementation costs and the ability to deliver high resolution content across distance continue to make analog video the preferred method for distributing full-motion video to LCD and plasma displays used in retail outlets, public spaces and KVM (keyboard, video and mouse) systems.
About the AD8175 and AD8176 crosspoint switches
The AD8175 (G=+2) and AD8176 (G=+4) triple 16x9 crosspoint switches deliver an industry-best bandwidth of 500 MHz, which is more than 60 percent faster than the nearest competitor, while offering twice the functionality. The switches feature a slew rate of 1800 V/µs to support UXGA or Ultra eXtended Graphics Array, a high monitor resolution of 1600 × 1200 pixels, which is quadruple the default resolution of SVGA (800 × 600), as well as QXGA or Quad eXtended Graphics Array, a superior resolution of 2048 x 1536. These devices also support sync on common-mode and sync on color operation. The AD8175/6 can be applied both differentially and single-ended. The new switches operate on a ±2.5V or +5V power supply and consume only 3.5 W. Their high level of integration, advanced architecture, and pin-out configuration simplify board layout and system design, while reducing cost.
Availability and Pricing
The AD8175 and AD8176 triple 16x9 crosspoint switches are sampling now and will be available in full production quantities in April and July 2007, respectively. The AD8175/6 are available in a 676-lead PBGA (plastic ball grid array) package over the extended industrial temperature range of -40 degrees C to +85 degrees C and are priced at $95 per unit in 100-unit quantities.
AD8145/6/7/8 differential amplifiers
The AD814x family of high-speed differential amplifiers is the industry’s first line of triple differential drivers and receivers to achieve full-power bandwidth of 550 MHz, or greater, which is more than twice the bandwidth of the nearest competitor. The wide bandwidth of the differential amplifiers complements the AD8175 switch by fully preserving the resolution of component video when sending and receiving signals across multi-stage video distribution systems. The ability to easily send and receive RGB and sync signals over Cat5 cable is integrated on one chip, enabling video distribution systems to maximize resolution at the lowest possible cost.
Availability and Pricing
The AD8145/6/7/8 differential amplifiers are sampling now. The AD8145 receiver is fully released to production, and the AD8146/7/8 drivers will be available in full production quantities in April 2007. The AD8145/6/7/8 are available in space-saving LFCSP (lead-frame chip-scale package) packages and are priced between $2.89 and $3.09 per unit in 1,000-unit quantities.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
Editor's Contact Information:
Sue Martenson
781-937-1989
781/937-1078
sue.martenson@analog.com