ANALOG DEVICES’ MIXED-SIGNAL FRONT END ICS REDUCE POWER AND PC BOARD SPACE IN WIRELESS COMMUNICATIONS EQUIPMENT

- Combined dual DAC and ADC devices harness ADI’s world-class 12-bit and 10-bit high-speed data conversion technology with analog peripherals to cut power consumption in femtocell and picocell wireless base stations by 40 percent.
Analog Devices Releases Two MXFEs for Femtocells

Norwood, MA (08/19/2010) - Analog Devices, Inc. (ADI), the leading supplier of data converters and global leader in high-performance semiconductors for signal-processing applications, today introduced 12-bit and 10-bit mixed-signal front-ends (MxFEs) that reduce power and board space for developers of wireless infrastructure and portable radio equipment. The 12-bit AD9963 and 10-bit AD9961 MxFEs use 40 percent less power and 25 percent less printed-circuit board area than competing devices without sacrificing performance. These MxFEs are especially effective for cost-sensitive wireless equipment, such as femtocell and picocell base stations that require highly integrated dual transmit-and-receive functions. For more information: visit http://www.analog.com/pr/AD9963 and http://www.analog.com/pr/AD9961.

“For RF design engineers designing small-scale wireless communication equipment, Analog Devices’ new MxFEs reduce power and component count,” said Chris Jacobs, product line director, Analog Devices. “The low-power, highly integrated transmit-and- receive paths of our new front-end ICs help customers simplify their designs to meet aggressive cost targets while still providing industry-leading data converter dynamic range.”

AD9963/1 Mixed-Signal Front End Key Features and Benefits

The 12-bit AD9963 and 10-bit AD9961 are pin-compatible, low-power MxFEs that each integrate two ADC (analog-to-digital converter) channels with sample rates to 100 MSPS (mega samples per second) and two DAC (digital-to-analog converter) channels with sample rates to 170 MSPS. The new MxFEs enable up to 10 dB better ACLR (adjacent-channel leakage ratio) performance than competing devices, easing design and filtering requirements while consuming less power.

Also integrated onto the devices are digital interfaces with flexible clocking options. These MxFEs have five auxiliary analog channels consisting of two 12-bit DACs, two 10-bit DACs and a 12-bit ADC. The ADC may be used to measure and monitor multiple points, both internal and external. The transmit path is configurable for 1x, 2x, 4x and 8x interpolation, and the receive path includes a by-passable 2x decimating low-pass filter. The AD9963 also integrates auxiliary LDO (low dropout) voltage regulators that allow the device to be powered from a single-supply and further reduce external component count.

Key features and benefits of the AD9963 and AD9961 MxFEs:

  • SNR (signal-to-noise ratio) = 66.5 dB
  • ACLR (adjacent-channel leakage ratio) = 72 dBc
  • Power = 425 mW at maximum sample rates
  • Transmit path power consumption = less than 100 mW at 170 MSPS @ 1.8 V
  • Receive path power consumption = less than 350 mW at 100 MSPS @ 1.8 V
  • Sleep and power-down modes
  • Supports full- and half-duplex data interfaces

The highly integrated MxFEs can be coupled with ADI’s ADF4602 3G multi-band transceiver, ADL5501 RMS power detector as well as RF amplifiers, such as the ADL5320, ADL5542 and ADL5601 products to create a complete femtocell radio.

Product Sample
Availability
Resolution
(Bits)
Power Price Each
Per 1,000
Packaging
AD9963 Now 12 425 mW $29.50 72-lead LFCSP
AD9961 Now 10 425 mW $25.75 72-lead LFCSP

More Information and Samples

Data Converters: Bridging the Analog and Digital Worlds

More designers turn to Analog Devices than any other supplier for the high-performance conversion technology required to bridge the analog and digital worlds in today’s myriad electronic systems. With the industry’s leading portfolio of ADCs (analog-to-digital converters) and DACs (digital-to-analog converters), Analog Devices’ converter products feature the right combination of sampling rates and accuracy with low noise, power, and price and small package size required by industrial, medical, automotive, communications, and consumer electronics. Online evaluation tools help customers quickly validate, select, and design in the optimal data converters to reduce design complexity, development schedules, and bill-of-material costs. To view ADI’s ADC selection guide, visit http://www.analog.com/ADCsearch . For ADC drivers, visit http://www.analog.com/ADCdrivers . To view ADI’s DAC selection guide, visit http://www.analog.com/DACsearch .

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Subscribe to ADI’s News Feed.

Follow ADI on: http://www.twitter.com/ADI_News.

Editor's Contact Information:

Bob Olson
781/937-1666

bob.olson@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close