INDUSTRY'S FIRST PRECISION HIGH-TEMPERATURE INSTRUMENTATION AMPLIFIER UNVEILED BY ANALOG DEVICES

Guaranteed to 210°C, the AD8229 is industry's first instrumentation amplifier designed and manufactured for hot, harsh and hostile environments.
Industry's First Precision High-Temperature Instrumentation Amplifier Unveiled by Analog Devices

Norwood, MA (03/08/2011) - The industry's first precision instrumentation amplifier designed and manufactured specifically for high temperature applications was unveiled today by Analog Devices, Inc. (ADI), a world leader in semiconductors for high-performance signal processing applications and leading supplier of signal conditioning technology. The AD8229, 1.0-nV/√Hz high-temperature instrumentation amplifier is the only low-noise instrumentation amplifier guaranteed to perform at up to 210°C in the most extreme environments, such as down-hole oil drilling, jet engines and space exploration. ADI Fellow Moshe Gerstenhaber explains how the AD8229 meets the design challenges of high-temperature environments in this video: http://www.youtube.com/watch?v=3ssOrdNAozs.

"The AD8229 is truly a breakthrough product for the oil exploration industry," said Jun Liu, General Manager of Qingdao Zitn Micro-electronics Co., Ltd. "It is not a retrofit of existing components. It was designed from the start for high-temperature environments. What this means to Zitn is that we will be able to operate our equipment longer with less repair time resulting in significant savings."

Until today's announcement, designers were forced to meet the challenges of rugged, noisy high-temperature environments with components not specifically designed for high-temperature conditions or were designed to operate at lower commercial grade temperatures. Often the repair and survival rates on systems using commercial-grade components are substandard, making them costly to maintain and operate. The AD8229 is unique because it solves some of the most difficult problems faced by engineers designing electronics for extreme hot, harsh and hostile environments to greatly improve maintenance and operation lifecycle.

The AD8229 instrumentation amplifier is best-in-class in all three performance categories for high-temperature applications, including CMRR (common mode rejection ratio), voltage offset and input noise. CMRR performance is 100 dB over the temperature range of -55°C to 210°C. The AD8229 input voltage offset varies by only 100-nV/°C over the entire temperate range. Input noise is 1.0-nV/√Hz making the amp ideal for sensors that read faint signals, such as those used in down-hole drilling, nuclear magnetic resonance spectroscopy and gamma ray detection.

AD8229 High-Temperature Instrumentation Amplifier Features:

  • Low Noise
    1.0-nV/√Hz Input Noise (max)
    45-nV/√Hz Output Noise (max)
  • High CMRR
    100-dB CMRR (minimum), G = 10
  • AC specifications
    15-MHz bandwidth (G = 1)
    25-V/µs slew rate
  • Low THD: 120dB (G=1) at 1 kHz
  • ±4-V to +18-V dual supply
  • Gain set with single resistor (G = 1 to 1000)

Availability and Pricing

Product Availability Temperature Range Price Each Per 1,000 Packaging
AD8229 Full volume production now -55°C to 210°C $120 8-lead CERDIP

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Bob Olson
781-937-1666

bob.olson@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close