HIGH COMMON-MODE VOLTAGE DIFFERENCE AMPLIFIER ENABLES DIRECT INTERFACE TO HIGH VOLTAGE INPUT UP TO ±600 V

Norwood, MA (05/03/2013) - Analog Devices, Inc. (ADI) today introduced the industry’s first precision difference amplifier to maintain excellent Common-Mode Rejection Ratio (CMRR) that exceeds 90dB at voltages up to ±600 V. Designed for applications such as motor control, process control and power supplies, the AD8479 enables accurate measurements of currents in the presence of voltage fluctuations as large as ±600 V without additional complex signal conditioning components.

The AD8479 guarantees to reject ±200V with ±5V power supplies. The AD8479 offers cost-effective isolation and can replace more costly devices in applications that do not require galvanic isolation. With higher than 90 dB CMRR, 130 kHz bandwidth, 2MΩ differential input impedance, within 0.02% gain error and 5ppm/°C gain drift, the AD8479 offers precision over a wide range of common-mode voltages and frequencies. It operates over an extended temperature range of -40°C to +125°C.

  • View the AD8479 product pages, download the data sheet and order samples.
  • Get your questions answered by ADI engineers on EngineerZone®, ADI’s online technical support community

Product Sample Availability Full Production Price Each in 1,000 Quantities Packaging
AD8479 Now Now $2.81 SOIC-8

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

To subscribe to ADI's News Feed

Follow ADI on Twitter

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

Editor's Contact Information:

Sarah Shieh
781-937-2572

sarah.shieh@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close