ArWest Communications Corporation


ArWest Employs Blackfin® in RadioTransceiver for SCADA Market

ArWest




Most consumers would be surprised to learn that their cellular phones are based on an old technology that their grandparents used in lieu of TV for entertainment - the old-fashioned radio. Today, there are over 1 billion digital cellular phones in use that are serviced by more than a million base stations. These cellular phones and base stations are actually sophisticated transmitters/receivers (transceivers). Unlike cellular radios and analog tuners of yesteryear, today's cellular phone devices are actually software-defined radios (SDRs) with coded radio functions executing on embedded microprocessors.

California-based ArWest Communications Corporation is putting this same class of radio technology to good use in the Supervisory Control and Data Acquisition (SCADA) market. The diverse applications of SCADA include asset-management for real-time inventory tracking; remote control/reporting within the utilities, oil/gas and water industries; crop monitoring and reporting for agriculture; Global Navigation Satellite System (GNSS) operations (which is a satellite-based radio navigation system that also uses ground-based systems to improve the accuracy of positional data); and wireless data systems for public safety and transportation to improve the flow of traffic. (Wireless data systems are typically used by dispatchers, police officers, emergency medical services and the military personnel.)

Typical SCADA Applications

ArWest Radio Tranceiver

As ArWest began to develop its transceiver aimed at the SCADA market, they searched for a processor with low power consumption that could handle both microcontroller (MCU) and signal processing tasks. ArWest chose the Blackfin ADSP-BF532 processor from Analog Devices, Inc. (ADI) because it exhibited the lowest power consumption in its class of processors. "Since our wireless communications systems are deployed in the field during rugged conditions," said Barrie Hogarth, Vice President of Marketing at ArWest, "low power consumption and high reliability are an absolute must."

Relying on Technology
As noted above, SCADA technology is a vital component within many industries from distribution to exploration to production. This technology enables work crews to be dispatched quickly to any problem area without the use of expensive leased lines, and it allows a user to monitor and control the processing and delivery of a product. In keeping with SCADA technology, wireless data communication must not only be reliable, it must also be cost-effective. Care must also be taken to minimize system interruptions and the costs associated with operational downtime.

ArWest set about to develop its VHF/UHF narrow-band radio transceiver using signal-processing technology originally developed for the cellular phone market. Ultimately, the company developed systems that can be managed, monitored and modified through the Internet. Basing its products on SDR, the company was also able to incorporate many other technologies, including high-level modulation techniques GMSK/BPSK, QPSK, 8PSK, and 16QAM that allow the user to achieve the highest data speed (over-the-air of 38400 bps at 25 kHz and 19200 bps at 12.5 kHz) for up to 50 miles.

"To meet our stringent design requirements, we wanted a processor with 240 MHz and power consumption less than 300 mW," said Hogarth. With performance of 240 MHz, the Blackfin ADSP-BF532 processor met ArWest's performance needs, and with the chip powered at 3.3 V, power dissipation was low enough to meet the company's stated requirements.

ArWest

Blackfin processors provide world-class power management and performance and are created in a low-power and low-voltage design. This family of processors features on-chip dynamic power management with the ability to vary both the voltage and the frequency of operation to significantly lower overall power consumption.

"We also wanted a chip that could handle both MCU and signal processing tasks simultaneously," said Gagik Harutyunyan, Chief Technology Officer at ArWest, "and Blackfin was ideal." Blackfin processors combine breakthrough signal-processing performance and power efficiency in a RISC programming model. The processors allow flexible resource allocation between hard real-time signal processing tasks and non-real-time control tasks, with system control tasks often running in the shadow of signal-processing tasks. Blackfin processors also include advanced memory management that support memory-protected embedded operating systems. ArWest used Express Logic's ThreadX real-time operating system to host the application.

Rich Set of Peripherals
ArWest's current line of AlphaWave (AW) radio modems are pre-configured to operate in the following frequency ranges: the AW400 operates in the 403 to 470 MHz band; the AW200 operates in the 220 to 235 MHz band; and the AW100 operates in the 150 to 170 MHz band. These products can be software configured with inter-channel spacing of 25, 12.5 or 6.25 kHz to eliminate cross talk. The AW400 can be configured to both "Transmit/Receive" or to "Receive Only." ArWest products transmit power of 100 mW to 35 W, complying with European Telecommunications Standards Institute (ETSI) regulations and Federal Communications Commission (FCC) regulations.

Distributed via Avnet, Inc.

These radio modems include other features such as selectable error correction, which improves the operation of the radio modems under interference, data scrambling, frequency hopping, low power consumption, sleep modes and plug-and-play installation for remote terminals. "There's no need for periodic calibrations as with older radio modems," said Hogarth. "Our new AlphaWave radio modems are ideal for meeting the varied conditions of SCADA users in a diversity of markets."

For tool support and to help facilitate its architecture evaluation, ArWest took advantage of ADI's EZ-Kit, which includes an evaluation board and VisualDSP++.

As ArWest prepares its next generation of AW products - a dedicated base station with a direct connection to Ethernet - Hogarth stated this design would include ADI's ADSP-BF537 Blackfin processor.

For more information about ArWest Communications, visit the company website.

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close