This code example gives the c code source files that allow configuration of the ADF7020 using an 8052 based microcontroller. Routines to write the configuration values to the ADF7020 are provided. The routines in this file will have to be adapted depending on the MCU and compiler used. This version uses the ADuC845/847 Microconverter form Analog Devices. The code was developed using the Keil C51 compiler within their uVision IDE.
This code example gives the c code that allows configuration of the ADF7020 using the ADSP-BF53X, Blackfin DSP processor. Routines to write the configuration values to the ADF7020 are provided as well as routines allowing a simple RF link to be setup between two ADF7020 devices. Please refer to Application Note AN-771 for details on the hardware connections.
This code provides low level device driver code, written in C, for the ADF7021 transceiver. The code can be tested using the EVAL-ADF70XXMB2 mother board plus EVAL-ADF7021DBX daughterboard. The device driver code size is < 4kbytes.
This code example gives the c code source files that allow configuration of the ADF7023 using an ARM7 based microcontroller. Routines to write the configuration values to the ADF7023 are provided. The routines in this file will have to be adapted depending on the MCU and compiler used. This version uses the ADuC7020 Microcontroller from Analog Devices.
© 1995 - Analog Devices, Inc. All Rights Reserved