Norwood, MA (11/09/2011) - Analog Devices, Inc. (ADI), a world leader in semiconductors for high-performance signal processing applications, will broadcast its latest webcast "Solutions for Fitting High Performance RF Signal Chains into Small Spaces" on November 16, 2011, at 12:00 pm EDT.
This webcast will focus on the challenges that non-handset-based wireless equipment designers face with the current state of integration of RF IC technology. Such challenges may include more functionality in smaller space, often with the added challenge of having to implement broadband transceivers that can be reused at multiple frequencies. Specific topics include the integration of high performance VCOs (voltage-controlled oscillator) into PLLs (phase lock loop), integrating signal chains horizontally vs. vertically and external vs. internal matching in RF Amplifiers.
Engineers who design RF signal chains using discrete components in the 10 MHz to 10 GHz frequency range.
Eamon Nash is an applications engineering manager in Analog Devices' RF Products Group. Over Eamon's 20 year career at Analog Devices, he has held a variety of positions including field applications engineer, covering mixed signal and DSP products, and applications engineer specializing in discrete RF components for wireless applications. Eamon graduated from the University of Limerick, Ireland with a Bachelor of Engineering degree in Electronics.
Register for ADI's webcast "Solutions for Fitting High Performance RF Signal Chains into Small Spaces" on November 16, 2011, 12:00 pm EDT.
Learn more about Analog Devices' RF IC products.
For additional support, connect with engineers and ADI product experts on EngineerZone™, an online technical support community.
ADI's webcasts cover topics relating to relevant challenges in designing with semiconductors and provide engineers with access to online design materials on a variety of solutions-oriented issues. Each webcast is followed by a Q&A and with the opportunity to download the presentation. For more than 45 years, ADI has been an engineering resource to help make it easier for customers to get their jobs done. To access the complete archive of webcasts for engineers, please visit: http://www.analog.com/pr/webcasts.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Subscribe to Analog Dialogue, ADI's monthly technical journal.
Howard Wisniowski
781-937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved