NEW MICROWAVE PLL SYNTHESIZER ELIMINATES FREQUENCY-DOUBLING IN BROADBAND, POINT-TO-POINT AND MULTIPOINT WIRELESS APPLICATIONS

ADF41020

Norwood, MA (10/11/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance signal processing technology and leading provider of RF ICs, today introduced a PLL (phase-locked loop) frequency synthesizer that can be used to implement local oscillators as high as 18 GHz in the up-conversion and down-conversion sections of wireless receivers and transmitters. The exceptionally high bandwidth of the ADF41020 allows designers to potentially eliminate a frequency-doubler stage, which simplifies system architecture and reduces cost in applications including microwave point-to-point and multi-point radios, wireless infrastructure equipment, VSAT (very small aperture terminal) radios, semiconductor test equipment, radar applications and private mobile radios. With an operating bandwidth up to 18GHz, this represents the highest frequency PLL available on the market today.

"The ADF41020 PLL is the latest addition to ADI's leading portfolio of phase locked loop synthesizers and extends our portfolio into higher frequency ranges," said Peter Real, vice president, Linear and RF products, Analog Devices. "This new PLL helps significantly reduces component count and system cost while continuously improving performance in next-generation radio designs."

The ADF41020 PLL frequency synthesizer consists of a low noise, digital phase frequency detector, a precision charge pump, a programmable reference divider and high-frequency programmable feedback dividers. A complete synthesizer can be implemented if the PLL is used with an external loop filter and VCO (voltage controlled oscillator). The PLL can be used to drive external microwave VCOs via an active loop filter. The pin-out matches very closely the pinout of the ADF4106/7/8 family of integer-N PLLs, meaning only a minor layout change is required when updating a design to take advantage of the much wider bandwidth.

ADF41020 PLL Frequency Synthesizer Key Features

  • 18-GHz maximum RF input frequency
  • Integrated prescaler
  • Programmable dual-modulus prescaler
  • 2.7-V to 3.3-V PLL power supply
  • Programmable charge pump currents
  • 3-wire serial interface
  • Analog and digital lock detect
  • Hardware and software power-down mode

Pricing, Availability and Complementary Products

Product Price Each in 1,000-unit Quantities Availability Package
ADF41020 $12.77 Samples available 20-lead LFCSP

The ADF41020 PLL frequency synthesizer is software compatible with the existing ADF4106, ADF4107 and ADF4108 PLLs and is well-suited for use with a variety of products including the ADP150 LDO (low dropout regulator) and the OP184 operational amplifier.

RF IC Portfolio Covers Entire RF Signal Chain

Using a unique combination of design skills, system understanding and process technologies, Analog Devices offers the broadest portfolio of RF ICs covering the entire RF signal chain from industry-leading high-performance RF function blocks to highly integrated WiMAX and short-range, single-chip transceiver solutions. The RF function blocks include PLL, integrated PLL/VCO and DDS synthesizers; TruPwr™ RMS power detectors and logarithmic amplifiers; variable gain amplifiers; power amplifiers, low noise amplifiers and other amplifiers; RF mixers and direct conversion modulator and demodulator products. These products are supported by a wide range of design resources to ease the development of RF systems, including free design tools, Circuits from the Lab™ reference circuits and the EngineerZone™ technical forums. For more information, visit http://www.analog.com/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index. http://www.analog.com

Follow ADI on Twitter at http://www.twitter.com/ADI_News

Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogdialogue

Editor's Contact Information:

Colleen Cronin
781-937-1622

colleen.cronin@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close